Hello experts,
I have question for total current capability. TLC59283 can drive max 45mAx16ch = 720mA if we ignore thermal problem? Or is ther any total current limit as device?
Thanks and best regards,
Ryo Akashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello experts,
I have question for total current capability. TLC59283 can drive max 45mAx16ch = 720mA if we ignore thermal problem? Or is ther any total current limit as device?
Thanks and best regards,
Ryo Akashi
Hi Ryo,
TLC59283 can drive max 45mAx16ch = 720mA if we ignore thermal problem?
Yes. This is the case when 3.6 V < VCC ≤ 5.5 V.
Or is ther any total current limit as device?
From the chip's perspective, there are no total current limit other than thermal concerns.
Best Regards,
Steven