Part Number: TPS65987EVM
Hello,
I have to design an interface between a PC that supports Thunderbolt and a system. One video signal and one audio signal are sent to the system from the PC, and there is a USB2 communication between both too (please see the attached image). Do you think I can use the TPS65987EVM to do this ? Three important questions :
-Will the PC work in display port alt mode even if it supports Thunderbolt ? I assume that if it supports Thunderbolt it will supports DP alt mode
-How can I get some audio signal from the USB signal ?
-The 10G-EXPANSION-EVM is not produced anymore and the page on the website no longer exists, is there a reason ? Is there an otheralternative ?
Regards
François