The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV627432: OCP test

Part Number: TLV627432

Hi team,

My customer test OCP and the waveforms are attached. When it is shorted, the current keeps at 800mA and the output voltage is pulled down to 62mV. I know that OCP is achieved by cycle-by-cycle detection. But why does the output voltage pull down? My customer still wants to know whether the device has life problem if it runs in OCP mode for a long time. As the temperature is high when OCP occurs, is there any safety problem?

Pic 1: Input current(Yellow line), Output voltage(Blue line) 

Pic 2: SW point waveform in OCP mode

Best Regards,

Peter

  • Hello Peter,

    Thank you for using E2E form.

    why does the output voltage pull down?

    You are applying the using the maximum current limit on the high side FET, which leads to limit the ON time of the high side FET, further leads low VOUT.

    cycle by cycle current protection works as mentioned in the datasheet.

    My customer still wants to know whether the device has life problem if it runs in OCP mode for a long time. As the temperature is high when OCP occurs, is there any safety problem?

    I don't see thermal shutdown option in this device, if you are running the device in OCP for long time, it might lead to increase the temperature of the device and if the device is operating beyond the recommended operating temperature conditions then their might be some reliability issues. 

    Thank you,

    Regards,

    Moheddin.