Other Parts Discussed in Thread: BQ25180
We are using BQ24073RGTT battery charger. In this pin no 2,3 (BAT1, BAT2) we have connected 10uF capacitor, a battery connector and we connected to the processor through the resistive divider to detect the battery detection or a dead battery detection. In this case, even though after removing the battery also we are receiving a floating data on the processor from the BAT1, BAT2 pins through the resistive divider. But we are expecting a LOW signal to be present since the battery is not connected but we are receiving floating data. Please help us on this.