Other Parts Discussed in Thread: TPS3898, BQ24780
Hi TI Teams,
We have some question about the application of BQ24780S when the battery pack does not have a BATPRES output pin. We have found a post about battery packs without BATPRES output pins, but still have some question.The details are shown as below:
E2E link:
Questions:
1) Did pin13 and pin14 of the BQ24780 have internal comparators? From the BQ24780S EVM schematic, we can see that there is an external independent comparator TPS3898 designed. If there is an internal comparator integrated, does it need to select only one of this external and internal comparator?
2) If the CMPIN and CMPOUT pin is used for detecting battery status, what needs to be set for SMBUS and how do the other registers need to be setting?
3) Does the R37 resistance value to 200KΩ is OK (the existing smart battery body detection pin has a 10K pull-down resistor)? And how to choose the R45 resistance value?
4) Does it possible to reactivate the battery by applying the CMPIN/CMPOUT pin in the case of battery overdischarge protection (battery voltage is 0)?
5) If the battery status is detected by the battery voltage at point 1, then pin13 and14 don't need to be used, can we directly using the battery voltage plus one MOSFET reverse processing to pin 15 can also realize the same function?
Thanks,
Kind Regards