In building a Cypress PSoC project, our entire project uses a 'Gnd' in many places.
In adding a BQ76920 and LiFePO4 4 cell battery pack is presenting problems.
Namely, the TI part (BQ76920) simplified schematic indicates 'Gnd' and Pack-, but the rest of the project appears to need to be powered by Pack+ & Pack-.
How do we go about changing the BQ76920 schematic snippet to fit into our project when 'Gnd' is used all over it, but that seems to be incorrect if 'Gnd' extends to the rest of the project?
Next, we are using an NCh MOSFET current mirror in the charging portion of the project to limit charging to 300mA as well as fusing and a main power switch between the battery pack and the circuitry.
There is some confusion generated by the 'Simplified Schematic' regarding where the current 'goes-ins' 'goes-outs' connections are in this topology.
Lastly, regarding the current sense resistor (Rsns) value... In using PCIFR18650-1500 cells from Zues (18650 cells limited to 4.5A max disch, 300mA nom charge), we are unsure what value should Rsns be considering OCD and SCD values unspecified by the manufacturer of the cells. We are considering 20mOhms.
Attached is the schematic page of our project's supply. It is in flux, because of the confusions listed above.
Recommendations?
Scott DeBruyn
Dutchman Electronics LLC