This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62A02A: Questions of TPS62A02A

Part Number: TPS62A02A
Other Parts Discussed in Thread: TPS62A03

Dear Team,

Do we have suitable solution can meet customer spec as below?

The solution is discreted.

1. 5V -> 0.95V (0.92v~0.98v), Io = 4.402A 

2. 5V -> 3.3V, Io = 2.235A

3. 3.3V -> 1V (0.97v~1.03v), Io = 1.719A

Many Thanks,

Jimmy