Other Parts Discussed in Thread: TMP303,
Hi Team,
We plan to use the BQ298012. We need to help confirm three questions:
2. Can pin5 of this IC support PTC function?
3.How is the maximum charger current and discharge current of IC calculated? 4mv/Rsns? Is there any requirement for Rsns resistance range? Can we use 0.5mΩ resistor to guarantee 8A charge and discharge current?
4.If the BQ298012 IC model is not suitable, we want to protect the 4.2V NMC cell, it also needs to support 0V charging function and charge and discharge current of not less than 6A, is there a more suitable IC recommended?