Dear...
I have some questions about what failure mode covered by some safety mechanisms, and how to deal with the fault detected by these safety mechanism.
- SM502 Short Comm Timeout Check: what failure mode covered by this SM? we have lost communication detection, why we still need this SM? and what reaction will need if detect SM502 fault?
- SM740 OTP ECC : why this SM is MPFDI, not a FDTI? I think the double bit error is a single point fault. What is the impact if have double bit error?
- SM403 OT/UT DAC Voltage Measurement and SM303 OV/UV DAC Voltage Measurement : What is the impact if detect DACs are not set correctly? and Does this SM fail will cause cell voltage protection/cell temperature protection failure?
- SM204 AUXADC Gain/Offset & Register Check and SM104 Vcell Gain/Offset & Register Check: in the description of these SMs, we need to use the registers CELLn_GAIN and CELLn_OFF / GPIOn_GAIN and GPIOn_OFF, and these registers are programmed at the TI factory. Why all registers's value are 0x00? Do these registers need to be calibrated at user's factory?If we don't use these GAIN and OFFSET because they are all empty, do we still need to implement these mechanisms? and what impact if we don't implement these SMs?
Thankyou.