Other Parts Discussed in Thread: TPS82671
If the Vin range is 3.6-4V, EN=1.2, and the temperature is 0-50 ℃ under a fixed 25 ° C condition:
Tps82673: What is the approximate ISD output of 1.8V?
Tps82671: What is the approximate ISD output of 1.26V?
Is this ISD mainly affected by temperature or input voltage range?