Other Parts Discussed in Thread: TPS546C23, TPS544C20
Tool/software:
The UV Warning and UV Fault thresholds are set to roughly 66% and 62% respectively of the Vref value (default settings). This seems somewhat low. Is this to provide margin to load transient events and prevent false triggers? I know the thresholds can be adjusted with PMBUS, but my application is not using PMBUS.
Also, is there any delay/deglitch time in the detection of UV (or OV) warning or fault to mask short transient events?