Tool/software:
Hi Christian,
Is it optional to use the ILIM pin as an input comes form from MCU which in turn :
1. Drive it to GND in order to cut off charging.
2. Release it to H-Z to let the resistors voltage divider on the ILIM pin to set the voltage on ILIM for the willing current limit and that way to enable back the charging.
If I do that, then what will be the output on the phase pin and on the HIDRV/LODRV when ILIM is short to GND?
Thanks,
Ohad