Tool/software:
Dear whom it may concern,
Hi, I am designing a half-bridge gatedriver circuit with a bias circuit to drive the 800V mosfet. The basic idea is to generate a biased 20V voltage across the GS pin of the mosfet when the input is high and generate a biased -4V voltage across the GS pin of the mosfet when the input is low. Now the circuit works fine without the Mosfet as attach TI simulation_HF_bias without mosfet. However, when I add the mosfet as TI simulation_HF_bias with mosfet, it keeps showing convergence problem. Can you please help me figure it out?
BTW, I failed to find any 800V MOSFET in your company website. Are you selling this kind of MOSFET?
Best regards,TI simulation_HF_bias without mosfet.tscTI simulation_HF_bias with mosfet.tsc
Wen Fankai