Hello,
The TPS65100 is not in SwitcherPro, so I can't estimate the input current requirement given Vin=5V with these output values. Is there a spreadsheet or other method of estimation?
Vout1 = 47mA max @ 9.84V
Vout2 = 1.8mA max @ -7V
Vout3 = 2.1mA max @ 19V
Vout4 = 21.3mA max @ 3.3V (using a MMBT4401 for Q1)
Thanks, in advance.
Scott