Dear TI team,
I am going to develop a product which must not show dangerous behaviour (=burning due to high current consumption) in case when LEDs reaches end of life. At the end of LEDs life there is a 50/50% risk that LEDs shortening the circuit.
The constant current version tlc59116 would be the best choice if there wouldn't be the heating disadvantage during normal operation. I know there are a lot of things you can do against it but at the end the tlc59116f is cooler due to design.
What happens, most likely, if the current of one ore more channel(s) of a tlc59116f increases to 500mA due to short circuit of a dying LED ?
Does it toogle betweem "Overtemperature-Off" and "On" state or is there a possibility that it burns down or simply loses this channel without losing all other channels ?
Thank you for your experienced answer in advance
regards
Gerd