This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2895: How limit the maximum duty cycle

Part Number: UCC2895

Hello,

I have a doubt regarding to the controller UCC2895. 

This controller has a 0 to 100% duty cycle control (phase shift in this case). Increasing CT limits the maximum duty cycle. However, the maximum value for CT according to the datasheet is 860pF and maximum duty cycle reduction in this case is very small.

Is there some way to limit the maximum duty cycle, for example to 95% or less?

Thanks a lot