The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TDA4VM: how to load MAIN core images from eMMC with boot_app

Part Number: TDA4VM

To enable fast CAN response, I need to use SBL to load MCU1_0 image (either AUTOSAR or TI-RTOS). 

boot_app_mcu_rtos is the demo app in SDK release for the early CAN response implementation. The boot app inside can be used to boot other cores in MAIN domain.

But the boot app reads the MAIN domain core images from OSPI flash. In my case, the MAIN domain core images may reside in eMMC.

How can I adapt this demo to achieve loading MAIN domain core images from eMMC(or SD)?

  • The u-boot is widely used across different platforms and different device vendors, the rich device/function supports are very useful. 

    We can use u-boot to achieve loading MAIN domain cores from eMMC or SD card. Either SPL or u-boot can be used.

    Here is an example based on SDK V7.3. It is validated with TDA4VM EVM.

    The boot flow which is achieved with the following patches can be figured as below:

    There are two patches for mcusw:

    patch 1: This patch is an adaption of running the default demo.

    Please adapt the PATH inside to match your environment setup.

    0001-adapt-local-environment-run-default-demo-pass.diff
    From d928305d3a0cb389f2d983b66fb1f02226419570 Mon Sep 17 00:00:00 2001
    From: Peter Li <a0220410@ti.com>
    Date: Fri, 18 Jun 2021 11:38:46 +0800
    Subject: [PATCH 1/2] adapt local environment, run default demo pass
    
    ---
     build/build_boot-app-mcu-rtos_release.sh      |   1 +
     .../scripts/hlos/constructappimageshlos.sh    |  22 ++-
     .../scripts/hlos/flash_ospi_boot_main_demo.sh | 158 ++++++++++++++++++
     .../scripts/makemulticore_j721e.sh            |   1 +
     4 files changed, 178 insertions(+), 4 deletions(-)
     create mode 100755 build/build_boot-app-mcu-rtos_release.sh
     create mode 100755 mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/flash_ospi_boot_main_demo.sh
     create mode 100755 mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/makemulticore_j721e.sh
    
    diff --git a/build/build_boot-app-mcu-rtos_release.sh b/build/build_boot-app-mcu-rtos_release.sh
    new file mode 100755
    index 0000000..87d687c
    --- /dev/null
    +++ b/build/build_boot-app-mcu-rtos_release.sh
    @@ -0,0 +1 @@
    +make -s -j can_boot_app_mcu_rtos HLOSBOOT=linux CANFUNC=none BOARD=j721e_evm SOC=j721e BUILD_PROFILE=release CORE=mcu1_0 BUILD_OS_TYPE=tirtos
    diff --git a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/constructappimageshlos.sh b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/constructappimageshlos.sh
    index 403ee60..99fa4bc 100755
    --- a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/constructappimageshlos.sh
    +++ b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/constructappimageshlos.sh
    @@ -4,10 +4,12 @@
     ##############################################################
     
     # MY_BOARD options are: j721e_evm or j7200_evm
    -MY_BOARD=$1
    +#MY_BOARD=$1
    +MY_BOARD=j721e_evm
     
     # OS options are: linux or qnx
    -OS=qnx
    +#OS=qnx
    +OS=linux
     
     # Linux-specific paths
     # --------------------
    @@ -17,7 +19,15 @@ OS=qnx
     # base-board.dtb (k3-j72*-common-proc-board.dtb), and Image files
     
     # Linux build directory containing all the locally-built Linux-related binaries
    -LINUX_BUILD_DIR_PATH=USER_DEFINED_PATH
    +if [ $OS == "linux" ]; then
    +   SDK_PATH=/home/a0220410local/Public/J721E/SDK_V7.3
    +
    +   PSDKRA_INSTALL_PATH=$SDK_PATH/ti-processor-sdk-rtos-j721e-evm-07_03_00_07
    +   PSDKLA_INSTALL_PATH=$SDK_PATH/ti-processor-sdk-linux-j7-evm-07_03_00_05
    +   LINUX_TOOLCHAIN_PATH_GCC_ARCH64=$PSDKRA_INSTALL_PATH/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/bin
    +   LINUX_PREBUILT_DIR=${PSDKLA_INSTALL_PATH}/board-support/prebuilt-images
    +   LINUX_BUILD_DIR_PATH=${PSDKLA_INSTALL_PATH}/board-support/u-boot_build/a72/spl
    +fi
     
     # QNX-specific paths
     # ------------------
    @@ -63,6 +73,10 @@ pushd $PWD > /dev/null
     if [ $OS == "linux" ]; then
         cd $LINUX_BUILD_DIR_PATH
         #cd $LINUX_PREBUILT_DIR_PATH
    +    cp $LINUX_PREBUILT_DIR/bl31.bin .
    +    cp $LINUX_PREBUILT_DIR/bl32.bin .
    +    cp $LINUX_PREBUILT_DIR/Image .
    +    cp $LINUX_PREBUILT_DIR/k3-j721e-common-proc-board.dtb base-board.dtb
     fi
     if [ $OS == "qnx" ]; then
         cd $QNX_PREBUILT_DIR_PATH
    @@ -73,7 +87,7 @@ for i in "${GenFiles[@]}"
     do
         echo "Generating $i image"
         if [ $OS == "linux" ]; then
    -        aarch64-none-linux-gnu-ld -T $LDS_PATH/$i.lds -o $MULTICOREAPP_BIN_PATH/$i.elf
    +        ${LINUX_TOOLCHAIN_PATH_GCC_ARCH64}/aarch64-none-linux-gnu-ld -T $LDS_PATH/$i.lds -o $MULTICOREAPP_BIN_PATH/$i.elf
         fi
         if [ $OS == "qnx" ]; then
             ${TOOLCHAIN_PATH_GCC_ARCH64}/aarch64-unknown-nto-qnx7.0.0-ld -T $LDS_PATH/$i.lds -o $MULTICOREAPP_BIN_PATH/$i.elf
    diff --git a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/flash_ospi_boot_main_demo.sh b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/flash_ospi_boot_main_demo.sh
    new file mode 100755
    index 0000000..0bdf1cc
    --- /dev/null
    +++ b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/flash_ospi_boot_main_demo.sh
    @@ -0,0 +1,158 @@
    +# Please refer to below link for OSPI image address
    +# https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/latest/exports/docs/mcusw/mcal_drv/docs/drv_docs/demo_boot_app_mcu_rtos_top.html
    +#
    +
    +#adjust blow PATH according to your own enviroment
    +export FLASH_TTY_PORT=/dev/ttyUSB1
    +export PSDKRA_PATH=/home/a0220410local/Public/J721E/SDK_V7.3/ti-processor-sdk-rtos-j721e-evm-07_03_00_07
    +export DSLITE_PATH=/home/a0220410local/Public/J721E/uniflash_6.2.0
    +export MCU_APP_PATH=$PSDKRA_PATH/mcusw/binary
    +export MAIN_APP_PATH=$PSDKRA_PATH/mcusw/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/binary/bin/j721e_evm
    +
    +#path used by utility
    +export PDK_PATH=$PSDKRA_PATH/pdk_jacinto_07_03_00_29
    +export FLASH_PROGRAMMER_BINARY=$PDK_PATH/packages/ti/board/utils/uniflash/target/bin/j721e_evm/uart_j721e_evm_flash_programmer_release.tiimage
    +export FLASH_PROGRAMMER_SYSFW=$PDK_PATH/packages/ti/board/utils/uniflash/target/bin/j721e_evm/sysfw.bin
    +export FLASH_PATTERN_BINARY=$PDK_PATH/packages/ti/board/src/flash/nor/ospi/nor_spi_patterns.bin
    +export SBL_CUST_BINARY=$PDK_PATH/packages/ti/boot/sbl/binary/j721e_evm/cust/bin/sbl_cust_img_mcu1_0_release.tiimage
    +export SBL_PATH=$PDK_PATH/packages/ti/boot/sbl/binary/j721e_evm/ospi/bin
    +export TIFS_BINARY=$PDK_PATH/packages/ti/drv/sciclient/soc/V1/tifs.bin
    +export MCU1_0_IMAGE=$MCU_APP_PATH/can_boot_app_mcu_rtos/bin/j721e_evm/can_boot_app_mcu_rtos_mcu1_0_release.appimage
    +export STAGE1_IMAGE=$MAIN_APP_PATH/multicore_MCU2_0_MCU2_1_stage1.appimage
    +export STAGE2_IMAGE=$MAIN_APP_PATH/multicore_DSPs_MCU3_0_MCU3_1_stage2.appimage
    +export ATF_OPTEE_IMAGE=$MAIN_APP_PATH/atf_optee.appimage
    +export KERNEL_IMAGE=$MAIN_APP_PATH/tikernelimage_linux.appimage
    +export DTB_IMAGE=$MAIN_APP_PATH/tidtb_linux.appimage
    +export CURRENT_PATH=$PWD
    +
    +echo "checking $TIFS_BINARY ..."
    +if [ ! -f $TIFS_BINARY ]; then
    +echo "ERROR!!! $TIFS_BINARY doesn't exist!!!"
    +exit 1
    +else
    +echo "$TIFS_BINARY is in place."
    +fi
    +
    +echo ""
    +echo "checking $FLASH_PATTERN_BINARY ..."
    +if [ ! -f $FLASH_PATTERN_BINARY ]; then
    +echo "ERROR!!! $FLASH_PATTERN_BINARY doesn't exist!!!"
    +exit 2
    +else
    +echo "$FLASH_PATTERN_BINARY is in place."
    +fi
    +
    +echo ""
    +echo "checking $FLASH_PROGRAMMER_BINARY ..."
    +if [ ! -f $FLASH_PROGRAMMER_BINARY ]; then
    +echo "$FLASH_PROGRAMMER_BINARY doesn't exist!!!"
    +echo " =============================================================================== "
    +echo " Please build flash programmer in $PDK_PATH/packages/ti/build"
    +echo " make PLATFORM=j721e_evm board_utils_uart_flash_programmer"
    +echo " =============================================================================== "
    +exit 3
    +fi
    +
    +echo ""
    +echo "checking $SBL_CUST_BINARY ..."
    +if [ ! -f $SBL_CUST_BINARY ]; then
    +echo "$SBL_CUST_BINARY doesn't exist, ATTENTION!!!"
    +echo " =============================================================================== "
    +echo " Please build the SBL in $PDK_PATH/package/ti/build "
    +echo " step 1: make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release pdk_libs_clean"
    +echo " step 2: make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release pdk_libs"
    +echo " step 3: make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_cust_img_clean"
    +echo " step 4: make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_cust_img"
    +echo " =============================================================================== "
    +exit 4
    +fi
    +
    +echo ""
    +echo "checking $MCU1_0_IMAGE ..."
    +if [ ! -f $MCU1_0_IMAGE ]; then
    +echo "$MCU1_0_IMAGE doesn't exist, ATTENTION!!!"
    +exit 5
    +fi
    +
    +echo ""
    +echo "all the necessary binaries are available, good to go..."
    +
    +echo ""
    +echo "checking $FLASH_PROGRAMMER_SYSFW ..."
    +if [ ! -f $FLASH_PROGRAMMER_SYSFW ]; then
    +echo "cp $TIFS_BINARY to $FLASH_PROGRAMMER_SYSFW"
    +cp $TIFS_BINARY $FLASH_PROGRAMMER_SYSFW
    +else
    +echo "$FLASH_PROGRAMMER_SYSFW is in place."
    +fi
    +
    +echo ""
    +echo "----step 1---- flash $FLASH_PROGRAMMER_BINARY ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $FLASH_PROGRAMMER_BINARY -i 0
    +
    +echo ""
    +echo "----step 2---- erase flash ..."
    +#erase flash, only needed once if FLASH layout isn't changed
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -e 3000000 -d 3 -o 0
    +
    +echo ""
    +echo "----step 3---- flash ospi pattern ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $FLASH_PATTERN_BINARY -d 3 -o 3FE0000
    +
    +echo ""
    +echo "----step 4---- flash SBL ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $SBL_CUST_BINARY -d 3 -o 0
    +
    +echo ""
    +echo "----step 5---- flash TIFS ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $TIFS_BINARY -d 3 -o 80000
    +
    +echo ""
    +echo "----step 6---- flash mcu1_0 image ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $MCU1_0_IMAGE -d 3 -o 100000
    +
    +echo ""
    +echo "----step 7---- flash stage1 image ..."
    +if [ ! -f $STAGE1_IMAGE ]; then
    +echo "$STAGE1_IMAGE doesn't exist, ATTENTION!!!"
    +exit 6
    +else
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $STAGE1_IMAGE -d 3 -o 1fc0000
    +fi
    +
    +echo ""
    +echo "----step 8---- flash stage2 image ..."
    +if [ ! -f $STAGE2_IMAGE ]; then
    +echo "$STAGE2_IMAGE doesn't exist, ATTENTION!!!"
    +exit 7
    +else
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $STAGE2_IMAGE -d 3 -o 27c0000
    +fi
    +
    +echo ""
    +echo "----step 9---- flash atf_optee image ..."
    +if [ ! -f $ATF_OPTEE_IMAGE ]; then
    +echo "$ATF_OPTEE_IMAGE doesn't exist, ATTENTION!!!"
    +exit 8
    +else
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $ATF_OPTEE_IMAGE -d 3 -o 1c0000
    +fi
    +	
    +echo ""
    +echo "----step 10---- flash kernel image ..."
    +if [ ! -f $KERNEL_IMAGE ]; then
    +echo "$KERNEL_IMAGE doesn't exist, ATTENTION!!!"
    +exit 9
    +else
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $KERNEL_IMAGE -d 3 -o 7c0000
    +fi
    +
    +echo ""
    +echo "----step 11---- flash dtb image ..."
    +if [ ! -f $DTB_IMAGE ]; then
    +echo "$DTB_IMAGE doesn't exist, ATTENTION!!!"
    +exit 10
    +else
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $DTB_IMAGE -d 3 -o 1ec0000
    +fi
    +
    diff --git a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/makemulticore_j721e.sh b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/makemulticore_j721e.sh
    new file mode 100755
    index 0000000..0ac7543
    --- /dev/null
    +++ b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/makemulticore_j721e.sh
    @@ -0,0 +1 @@
    +./makemulticore.sh j721e_evm
    -- 
    2.17.1
    
    

    Steps for running the default demo:

         1. use the build_boot-app-mcu-rtos_release.sh to build MCU1_0 image.

         2. use the makemulticore_j721e.sh to build multicore images used in this demo

         3. use the constructappimageshlos.sh to create HLOS images. In this demo, we are using prebuilt images in the SDK.

         4. use flash_ospi_boot_main_demo.sh to flash the above images to OSPI flash.

    ----------------------------------------------------------------------------------

    With the patch 1 above, we can run the SDK default demo with TDA4VM EVM. Now can use patch2 to do the u-boot-spl loading via boot_app.

    patch 2: this patch is based on patch 1.

    0002-boot-app-load-u-boot-spl.diff
    From 81b62127c287748ee638d939ca1f791bf0ea4b72 Mon Sep 17 00:00:00 2001
    From: Peter Li <a0220410@ti.com>
    Date: Fri, 18 Jun 2021 14:13:09 +0800
    Subject: [PATCH 2/2] boot app load u-boot-spl
    
    ---
     build/build_boot-app-mcu-rtos_release.sh      |   2 +-
     mcuss_demos/boot_app_mcu_rtos/boot.c          |   2 +
     .../scripts/hlos/constructappimageshlos.sh    |   3 +-
     .../hlos/flash_ospi_boot_u-boot-spl.sh        | 131 ++++++++++++++++++
     .../scripts/hlos/linux/tiubootspl_linux.lds   |  18 +++
     .../scripts/hlos/rebuild_ubootspl.sh          |  15 ++
     mcuss_demos/boot_app_mcu_rtos/makefile        |   9 +-
     .../soc/j721e/boot_core_defs.c                |  49 +++++++
     8 files changed, 225 insertions(+), 4 deletions(-)
     create mode 100755 mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/flash_ospi_boot_u-boot-spl.sh
     create mode 100755 mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/linux/tiubootspl_linux.lds
     create mode 100755 mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/rebuild_ubootspl.sh
    
    diff --git a/build/build_boot-app-mcu-rtos_release.sh b/build/build_boot-app-mcu-rtos_release.sh
    index 87d687c..32ed8c7 100755
    --- a/build/build_boot-app-mcu-rtos_release.sh
    +++ b/build/build_boot-app-mcu-rtos_release.sh
    @@ -1 +1 @@
    -make -s -j can_boot_app_mcu_rtos HLOSBOOT=linux CANFUNC=none BOARD=j721e_evm SOC=j721e BUILD_PROFILE=release CORE=mcu1_0 BUILD_OS_TYPE=tirtos
    +make -s -j can_boot_app_mcu_rtos HLOSBOOT=linux BOOTMODE=ospi BOOTUBOOTSPL=enabled CANFUNC=none BOARD=j721e_evm SOC=j721e BUILD_PROFILE=release CORE=mcu1_0 BUILD_OS_TYPE=tirtos
    diff --git a/mcuss_demos/boot_app_mcu_rtos/boot.c b/mcuss_demos/boot_app_mcu_rtos/boot.c
    index b748757..b19a3e8 100755
    --- a/mcuss_demos/boot_app_mcu_rtos/boot.c
    +++ b/mcuss_demos/boot_app_mcu_rtos/boot.c
    @@ -400,10 +400,12 @@ static int32_t OSPIBootStageImage(sblEntryPoint_t *pEntry, uint32_t address)
     #        if defined(LINUX_OS)
                     else
                     {
    +#if         !defined(BOOT_UBOOT_SPL)
                         status = OSPIBootImageLate(&k3xx_evmEntry, OSPI_OFFSET_A72IMG3);
                         if (status != E_PASS)
                             AppUtils_Printf(MSG_NORMAL,
                                             "Error parsing A72 appimage #3 for HLOS boot\n");
    +#           endif
                     }
     #        endif
                 }
    diff --git a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/constructappimageshlos.sh b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/constructappimageshlos.sh
    index 99fa4bc..27fc813 100755
    --- a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/constructappimageshlos.sh
    +++ b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/constructappimageshlos.sh
    @@ -57,8 +57,7 @@ LDS_PATH=${PWD}/${OS}
     # Defines which appimages this script will create
     if [ $OS == "linux" ]; then
         GenFiles=("atf_optee" \
    -              "tidtb_linux" \
    -              "tikernelimage_linux"
    +              "tiubootspl_linux"
                  );
     fi
     if [ $OS == "qnx" ]; then
    diff --git a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/flash_ospi_boot_u-boot-spl.sh b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/flash_ospi_boot_u-boot-spl.sh
    new file mode 100755
    index 0000000..bd2eda0
    --- /dev/null
    +++ b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/flash_ospi_boot_u-boot-spl.sh
    @@ -0,0 +1,131 @@
    +# Please refer to below link for OSPI image address
    +# https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/latest/exports/docs/mcusw/mcal_drv/docs/drv_docs/demo_boot_app_mcu_rtos_top.html
    +#
    +
    +#adjust blow PATH according to your own enviroment
    +export FLASH_TTY_PORT=/dev/ttyUSB1
    +export PSDKRA_PATH=/home/a0220410local/Public/J721E/SDK_V7.3/ti-processor-sdk-rtos-j721e-evm-07_03_00_07
    +export DSLITE_PATH=/home/a0220410local/Public/J721E/uniflash_6.2.0
    +export MCU_APP_PATH=$PSDKRA_PATH/mcusw/binary
    +export MAIN_APP_PATH=$PSDKRA_PATH/mcusw/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/binary/bin/j721e_evm
    +
    +#path used by utility
    +export PDK_PATH=$PSDKRA_PATH/pdk_jacinto_07_03_00_29
    +export FLASH_PROGRAMMER_BINARY=$PDK_PATH/packages/ti/board/utils/uniflash/target/bin/j721e_evm/uart_j721e_evm_flash_programmer_release.tiimage
    +export FLASH_PROGRAMMER_SYSFW=$PDK_PATH/packages/ti/board/utils/uniflash/target/bin/j721e_evm/sysfw.bin
    +export FLASH_PATTERN_BINARY=$PDK_PATH/packages/ti/board/src/flash/nor/ospi/nor_spi_patterns.bin
    +export SBL_CUST_BINARY=$PDK_PATH/packages/ti/boot/sbl/binary/j721e_evm/cust/bin/sbl_cust_img_mcu1_0_release.tiimage
    +export SBL_PATH=$PDK_PATH/packages/ti/boot/sbl/binary/j721e_evm/ospi/bin
    +export TIFS_BINARY=$PDK_PATH/packages/ti/drv/sciclient/soc/V1/tifs.bin
    +export MCU1_0_IMAGE=$MCU_APP_PATH/can_boot_app_mcu_rtos/bin/j721e_evm/can_boot_app_mcu_rtos_mcu1_0_release.appimage
    +export STAGE1_IMAGE=$MAIN_APP_PATH/multicore_MCU2_0_MCU2_1_stage1.appimage
    +export STAGE2_IMAGE=$MAIN_APP_PATH/multicore_DSPs_MCU3_0_MCU3_1_stage2.appimage
    +export ATF_OPTEE_IMAGE=$MAIN_APP_PATH/atf_optee.appimage
    +export KERNEL_IMAGE=$MAIN_APP_PATH/tikernelimage_linux.appimage
    +export DTB_IMAGE=$MAIN_APP_PATH/tidtb_linux.appimage
    +export UBOOTSPL_IMAGE=$MAIN_APP_PATH/tiubootspl_linux.appimage
    +export CURRENT_PATH=$PWD
    +
    +echo "checking $TIFS_BINARY ..."
    +if [ ! -f $TIFS_BINARY ]; then
    +echo "ERROR!!! $TIFS_BINARY doesn't exist!!!"
    +exit 1
    +else
    +echo "$TIFS_BINARY is in place."
    +fi
    +
    +echo ""
    +echo "checking $FLASH_PATTERN_BINARY ..."
    +if [ ! -f $FLASH_PATTERN_BINARY ]; then
    +echo "ERROR!!! $FLASH_PATTERN_BINARY doesn't exist!!!"
    +exit 2
    +else
    +echo "$FLASH_PATTERN_BINARY is in place."
    +fi
    +
    +echo ""
    +echo "checking $FLASH_PROGRAMMER_BINARY ..."
    +if [ ! -f $FLASH_PROGRAMMER_BINARY ]; then
    +echo "$FLASH_PROGRAMMER_BINARY doesn't exist!!!"
    +echo " =============================================================================== "
    +echo " Please build flash programmer in $PDK_PATH/packages/ti/build"
    +echo " make PLATFORM=j721e_evm board_utils_uart_flash_programmer"
    +echo " =============================================================================== "
    +exit 3
    +fi
    +
    +echo ""
    +echo "checking $SBL_CUST_BINARY ..."
    +if [ ! -f $SBL_CUST_BINARY ]; then
    +echo "$SBL_CUST_BINARY doesn't exist, ATTENTION!!!"
    +echo " =============================================================================== "
    +echo " Please build the SBL in $PDK_PATH/package/ti/build "
    +echo " step 1: make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release pdk_libs_clean"
    +echo " step 2: make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release pdk_libs"
    +echo " step 3: make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_cust_img_clean"
    +echo " step 4: make BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_cust_img"
    +echo " =============================================================================== "
    +exit 4
    +fi
    +
    +echo ""
    +echo "checking $MCU1_0_IMAGE ..."
    +if [ ! -f $MCU1_0_IMAGE ]; then
    +echo "$MCU1_0_IMAGE doesn't exist, ATTENTION!!!"
    +exit 5
    +fi
    +
    +echo ""
    +echo "all the necessary binaries are available, good to go..."
    +
    +echo ""
    +echo "checking $FLASH_PROGRAMMER_SYSFW ..."
    +if [ ! -f $FLASH_PROGRAMMER_SYSFW ]; then
    +echo "cp $TIFS_BINARY to $FLASH_PROGRAMMER_SYSFW"
    +cp $TIFS_BINARY $FLASH_PROGRAMMER_SYSFW
    +else
    +echo "$FLASH_PROGRAMMER_SYSFW is in place."
    +fi
    +
    +echo ""
    +echo "----step 1---- flash $FLASH_PROGRAMMER_BINARY ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $FLASH_PROGRAMMER_BINARY -i 0
    +
    +echo ""
    +echo "----step 2---- erase flash ..."
    +#erase flash, only needed once if FLASH layout isn't changed
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -e 3000000 -d 3 -o 0
    +
    +echo ""
    +echo "----step 3---- flash ospi pattern ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $FLASH_PATTERN_BINARY -d 3 -o 3FE0000
    +
    +echo ""
    +echo "----step 4---- flash SBL ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $SBL_CUST_BINARY -d 3 -o 0
    +
    +echo ""
    +echo "----step 5---- flash TIFS ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $TIFS_BINARY -d 3 -o 80000
    +
    +echo ""
    +echo "----step 6---- flash mcu1_0 image ..."
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $MCU1_0_IMAGE -d 3 -o 100000
    +
    +echo ""
    +echo "----step 7---- flash atf_optee image ..."
    +if [ ! -f $ATF_OPTEE_IMAGE ]; then
    +echo "$ATF_OPTEE_IMAGE doesn't exist, ATTENTION!!!"
    +exit 6
    +else
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $ATF_OPTEE_IMAGE -d 3 -o 1c0000
    +fi
    +
    +echo ""
    +echo "----step 8---- flash u-boot-spl image ..."
    +if [ ! -f $UBOOTSPL_IMAGE ]; then
    +echo "$UBOOTSPL_IMAGE doesn't exist, ATTENTION!!!"
    +exit 7
    +else
    +$DSLITE_PATH/dslite.sh --mode processors -c $FLASH_TTY_PORT -f $UBOOTSPL_IMAGE -d 3 -o 7c0000
    +fi
    diff --git a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/linux/tiubootspl_linux.lds b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/linux/tiubootspl_linux.lds
    new file mode 100755
    index 0000000..a5d6519
    --- /dev/null
    +++ b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/linux/tiubootspl_linux.lds
    @@ -0,0 +1,18 @@
    +/*
    + * tiubootspl_linux.lds - simple linker file for stand-alone Linux kernel booting
    + *
    + * Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/
    + *
    + * Use of this source code is governed by a BSD-style license that can be
    + * found in the LICENSE.txt file.
    + */
    +OUTPUT_FORMAT("elf64-littleaarch64")
    +OUTPUT_ARCH(aarch64)
    +TARGET(binary)
    +INPUT(u-boot-spl.bin)
    +SECTIONS
    +{
    + . = 0x0000000080080000;
    + spl = .;
    + .spl : { u-boot-spl.bin }
    +}
    diff --git a/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/rebuild_ubootspl.sh b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/rebuild_ubootspl.sh
    new file mode 100755
    index 0000000..08218c4
    --- /dev/null
    +++ b/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/rebuild_ubootspl.sh
    @@ -0,0 +1,15 @@
    +export PSDK_PATH=/home/a0220410local/Public/J721E/SDK_V7.3
    +
    +export PSDKRA_PATH=$PSDK_PATH/ti-processor-sdk-rtos-j721e-evm-07_03_00_07
    +export PSDKLA_PATH=$PSDK_PATH/ti-processor-sdk-linux-j7-evm-07_03_00_05
    +export CURR_PATH=$PWD
    +
    +# Preserve original working directory
    +pushd $PWD > /dev/null
    +
    +cd $PSDKLA_PATH
    +make u-boot_clean
    +make u-boot
    +
    +# Restore shell to original working directory
    +popd > /dev/null
    diff --git a/mcuss_demos/boot_app_mcu_rtos/makefile b/mcuss_demos/boot_app_mcu_rtos/makefile
    index 60f329f..00e4a4e 100755
    --- a/mcuss_demos/boot_app_mcu_rtos/makefile
    +++ b/mcuss_demos/boot_app_mcu_rtos/makefile
    @@ -22,7 +22,11 @@ BISTFUNC ?= disabled
     #Setting BISTFUNC to enabled is only supported on j721e
     #BISTFUNC ?= enabled
     
    -$(info Building MCUSW CAN Boot App with BISTFUNC=$(BISTFUNC), BOOTFUNC=$(BOOTFUNC), HLOSBOOT=$(HLOSBOOT), BOOTMODE=$(BOOTMODE), CANFUNC=$(CANFUNC) and MCUONLYFUNC=$(MCUONLYFUNC))
    +# boot u-boot-spl options are enabled or disabled
    +BOOTUBOOTSPL ?= enabled
    +#BOOTUBOOTSPL ?= disabled
    +
    +$(info Building MCUSW CAN Boot App with BISTFUNC=$(BISTFUNC), BOOTFUNC=$(BOOTFUNC), HLOSBOOT=$(HLOSBOOT), BOOTMODE=$(BOOTMODE), BOOTUBOOTSPL=$(BOOTUBOOTSPL) CANFUNC=$(CANFUNC) and MCUONLYFUNC=$(MCUONLYFUNC))
     
     BUILD_OS_TYPE=tirtos
     include $(MCUSW_INSTALL_PATH)/build/Rules.make
    @@ -203,6 +207,9 @@ endif
     ifeq ($(HLOSBOOT), linux)
         CFLAGS_LOCAL_COMMON += -DMPU1_HLOS_BOOT_ENABLED -DLINUX_OS
         #CFLAGS_LOCAL_COMMON += -DMPU1_HLOS_BOOT_ONLY_ENABLED -DLINUX_OS
    +    ifeq ($(BOOTUBOOTSPL), enabled)
    +        CFLAGS_LOCAL_COMMON += -DBOOT_UBOOT_SPL
    +    endif
     else ifeq ($(HLOSBOOT), qnx)
         CFLAGS_LOCAL_COMMON += -DMPU1_HLOS_BOOT_ENABLED -DQNX_OS
         #CFLAGS_LOCAL_COMMON += -DMPU1_HLOS_BOOT_ONLY_ENABLED -DQNX_OS
    diff --git a/mcuss_demos/boot_app_mcu_rtos/soc/j721e/boot_core_defs.c b/mcuss_demos/boot_app_mcu_rtos/soc/j721e/boot_core_defs.c
    index 5b8e7be..d051b35 100644
    --- a/mcuss_demos/boot_app_mcu_rtos/soc/j721e/boot_core_defs.c
    +++ b/mcuss_demos/boot_app_mcu_rtos/soc/j721e/boot_core_defs.c
    @@ -156,17 +156,31 @@ const sblSlaveCoreInfo_t sbl_late_slave_core_stages_info[NUM_BOOT_STAGES][MAX_CO
         {
             /* MCU2_CPU0 info */
             {
    +#ifdef BOOT_UBOOT_SPL
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE
    +#else
             SBL_PROC_ID_MCU2_CPU0,
             SBL_DEV_ID_MCU2_CPU0,
             SBL_CLK_ID_MCU2_CPU0,
             SBL_MCU2_CPU0_FREQ_HZ,
    +#endif
             },
             /* MCU2_CPU1 info */
             {
    +#ifdef BOOT_UBOOT_SPL
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE
    +#else
             SBL_PROC_ID_MCU2_CPU1,
             SBL_DEV_ID_MCU2_CPU1,
             SBL_CLK_ID_MCU2_CPU1,
             SBL_MCU2_CPU1_FREQ_HZ,
    +#endif
             },
             {
             SBL_INVALID_CORE,
    @@ -192,38 +206,73 @@ const sblSlaveCoreInfo_t sbl_late_slave_core_stages_info[NUM_BOOT_STAGES][MAX_CO
         {
             /* MCU3_CPU0 info */
             {
    +#ifdef BOOT_UBOOT_SPL
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE
    +#else
             SBL_PROC_ID_MCU3_CPU0,
             SBL_DEV_ID_MCU3_CPU0,
             SBL_CLK_ID_MCU3_CPU0,
             SBL_MCU3_CPU0_FREQ_HZ,
    +#endif
             },
             /* MCU3_CPU1 info */
             {
    +#ifdef BOOT_UBOOT_SPL
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE
    +#else
             SBL_PROC_ID_MCU3_CPU1,
             SBL_DEV_ID_MCU3_CPU1,
             SBL_CLK_ID_MCU3_CPU1,
             SBL_MCU3_CPU1_FREQ_HZ,
    +#endif
             },
             /* DSP1_C66X info */
             {
    +#ifdef BOOT_UBOOT_SPL
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE
    +#else
             SBL_PROC_ID_DSP1_C66X,
             SBL_DEV_ID_DSP1_C66X,
             SBL_CLK_ID_DSP1_C66X,
             SBL_DSP1_C66X_FREQ_HZ,
    +#endif
             },
             /* DSP2_C66X info */
             {
    +#ifdef BOOT_UBOOT_SPL
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE
    +#else
             SBL_PROC_ID_DSP2_C66X,
             SBL_DEV_ID_DSP2_C66X,
             SBL_CLK_ID_DSP2_C66X,
             SBL_DSP2_C66X_FREQ_HZ,
    +#endif
             },
             /* DSP1_C7X info */
             {
    +#ifdef BOOT_UBOOT_SPL
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE,
    +        SBL_INVALID_CORE
    +#else
             SBL_PROC_ID_DSP1_C7X,
             SBL_DEV_ID_DSP1_C7X,
             SBL_CLK_ID_DSP1_C7X,
             SBL_DSP1_C7X_FREQ_HZ,
    +#endif
             },
         },
         {
    -- 
    2.17.1
    
    

    patch for u-boot:

    0001-Hack-force-u-boot-spl-to-boot-from-SD-card.diff
    From 4b7f8ffc9b33e762e99abaec7a3695bdc752f211 Mon Sep 17 00:00:00 2001
    From: Peter Li <a0220410@ti.com>
    Date: Fri, 18 Jun 2021 16:41:39 +0800
    Subject: [PATCH] Hack, force u-boot-spl to boot from SD card
    
    ---
     arch/arm/mach-k3/j721e_init.c | 8 ++++++++
     1 file changed, 8 insertions(+)
    
    diff --git a/arch/arm/mach-k3/j721e_init.c b/arch/arm/mach-k3/j721e_init.c
    index ea44bf57..f3120670 100644
    --- a/arch/arm/mach-k3/j721e_init.c
    +++ b/arch/arm/mach-k3/j721e_init.c
    @@ -720,6 +720,13 @@ static u32 __get_primary_bootmedia(u32 main_devstat, u32 wkup_devstat)
     
     u32 spl_boot_device(void)
     {
    +#if 1
    +	/* hack for SBL boot uboot-spl, we have already booted SBL from SPI
    +	 * we are going to boot uboot from MMCSD, MMC2 */
    +	printf("spl_boot_device: hack to boot from SD card\n");
    +
    +	return BOOT_DEVICE_MMC2;
    +#else
     	u32 wkup_devstat = readl(CTRLMMR_WKUP_DEVSTAT);
     	u32 main_devstat;
     
    @@ -735,6 +742,7 @@ u32 spl_boot_device(void)
     		return __get_primary_bootmedia(main_devstat, wkup_devstat);
     	else
     		return __get_backup_bootmedia(main_devstat);
    +#endif
     }
     #endif
     
    -- 
    2.17.1
    
    

    Steps to run:

        1) clean the mcusw binaries, build the boot_app_mcu_rtos via build_boot-app-mcu-rtos_release.sh

        2) build the u-boot-spl via rebuild_ubootspl.sh

        3) use the constructappimageshlos.sh to create u-boot-spl appimage.

        4) use flash_ospi_boot_u-boot-spl.sh to flash the binaries into OSPI flash

    There are other details we should take care of. Such as the building of cust_sbl, flash_programmer, etc.

    Please refer to https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/07_03_00_07/exports/docs/mcusw/mcal_drv/docs/drv_docs/demo_boot_app_mcu_rtos_top.html.