Other Parts Discussed in Thread: AM3359
Hi,
I am trying to use this board to implement acontis EtherCAT function.
I try to implement EC-Master (not based on TCP/IP) with CPSW mode and RAS-Server (based on TCP/IP) with ICSS mode.
I try to connect pin1 and pin2 for J18, and connect pin2 and pin3 for J19 as the picture below.
But acontis told me that TMDSICE3359 cannot support CPSW+ICSS mode, it can only support 2*CPSW or 2*ICSS. In another word, I can only connect pin1 and pin2 or pin2 and pin3 for J18,J19 at the same time.
My question is:
1. Whether J18 and J19 can be set separately? e.g. connect pin1 and pin2 for J18, and connect pin2 and pin3 for J19.
2. If question 1 not possible, what is the reason?
3. If question 1 not possible, this shortage is for TMDSICE3359 board or for AM3359 chip?
Thank you.