The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] PROCESSOR-SDK-TDAX: Flip/Mirror support in the display node

Part Number: PROCESSOR-SDK-TDAX

Is it possible to flip/mirror the source image on-the-fly along the x/y-axis to create a mirror effect on the source data?

  • The DISPC supports on-the-fly source image flip along the x/y-axis to create a mirror effect on the source data.
    The below 3 patches could be used in order to make use of this feature.

    The patches are created on top of SDK 07_03_00_07

    1. TIOVX_Flip_Support.patch 

    In the process function of the display node, the buffer address to be assigned to Fvid queue should be as follow for respective flip options:

         a. No Flip        : No change in the buffer base address.

         b. Vertical Flip : No change in the buffer base address. 

         c. Horizontal Flip :  Buffer base address should point to Start of last line of the window

         d. Both Vertical and horizontal flip : Buffer base address should point to Start of last line of the window

    In the control function of the display node, new control command "TIVX_DISPLAY_SELECT_FLIP" is added in order to accept the flip command from the HOST.

    This control command uses pointer to structure tivx_display_fliptype_t as an input argument.

    Valid values for the flip type are as shown below :
     0 : No Flip
     1 : Horizontal Flip (Along Y-axis)
     2 : Vertical Flip (Along X-axis)
     3 : Horizontal + Vertical Flip


    TIOVX_Flip_Support.patch

    2. PDK_Flip_Support.patch

    Correction in the increment value done for Horizontal flip.
    The correct value to the widthInBytes is  widthInBytes + pipeCfg->inFmt.pitch[0] - 1.

    Added CSL_DSS_VID1_ATTRIBUTES_FLIP_VAL_NOFLIP in case of No Flip option

    PDK_Flip_Support.patch

    3. Vision_Apps_Flip_Support.patch

    Created additional user interface for flipping the source image by the user.

    User could enter 'f' and then the corresponding flip type required as shown below :

    v: Vertical Flip
    h: Horizontal Flip
    f: Full Flip
    n: No Flip

    Once the fliptype is selected, the Host send the information to the display node and the source image is flipped on the display.

    VisionApps_Flip_Support.patch

    Please find the patches for SDK 8.2 below

    Flip_support_8_2.zip