This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713B: The program does not run even if I press the green execution button.

Guru 11060 points
Part Number: TMS320C6713B
Hi,
I am using C6713 DSK. I'm using CCS v3.3 on Windows XP, but I'm thinking of making it available for CCS V6.2 on Windows 10 as well. So, after creating a new CCS project, I created Hello World to check the operation. After Clean and Build, Debug and Transfer to DSK is completed. However, the program does not start even if I press the green execution button. There are no errors, and the console just says Build Finish. Is there anything I should check or is there a solution?
Thanks,
Eevee