This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VE-Q1: tda4ve 8.4 sdk edp

Part Number: TDA4VE-Q1

Hi Team,

The environment of the board we use is: SDK of tda4ve j721s2 version 8.4. We use the edp interface on the board for output and use the edp->hdmi converter. The crystal oscillator used on the board is 24MHz. I've changed the definition in the drv/dss/src/ file to 24MHz, but there are still some problems.

1. In the log of vision_apps, I can see that the display has been detected: DSS: isDpConnected = true. But there is nothing displayed on the screen when I run './run_app_dof.sh'.

2. Have you verified the 24MHz crystal oscillator input? After I open the REF_CLK_24MHz definition, the default pdk compilation will report an error.

Kind regards,

Katherine