Hello.
I'm developing custom board which has RMII connection with Ethernet Switch IC.
The AM62A and the Ethernet switch IC are connected via MAC-to-MAC mode.
The message 'eth0 Link is up' appears, but the ping command fails.
I suspect there may be a timing issue with the RMII TXD line.
After measuring with an oscilloscope, the output delay of the RMII_TXD line is approximately 4ns, whereas the output delay specification of the Ethernet switch IC is a minimum of 6ns.
Is is possible to adjust the output delay time of the RMII TXD?
Please refer to "Table 7-32. RMII[x]_TXD[1:0], and RMII[x]_TX_EN Switching Characteristics – RMII Mode" of AM62Ax Sitara Processors Data Sheet datasheet (Rev. A)
Thank you.
Best regards.