Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi Expert,
Could you help to provide Pinmux excel file for AX62XX?
SysConfig Tool export csv file does not list MUX Mode.
TDAV4VM provides MUX Mode
Thanks
Daniel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paul
AM62XX SysConfig export to csv file only lists the functions in use, and does not list the MUX mode of the CPU ball pad in use.
I don’t know the other functions of MUX mode of each CPU BALL.
If customers design their own chassis, they need to provide some information. Some customers' chassis specifications are not the same as the original design, so Mux mode information is required.
Thanks
Daniel
AM62XX SysConfig export to csv file only lists the functions in use, and does not list the MUX mode of the CPU ball pad in use.
The CSV file contains this information. For example, a snippet from the output csv (colorized) ...
Yellow is the pad name
Blue is the bull number
Green is the selected mux signal
Orange is the selected mux mode.
I don’t know the other functions of MUX mode of each CPU BALL.
The full mux functions are detailed in the device datasheet, section 6.2, Pin Attributes.
If customers design their own chassis, they need to provide some information. Some customers' chassis specifications are not the same as the original design, so Mux mode information is required.
I have attached a pinmux spreadsheet with this information. However.....
--Paul
Hi Paul
AM62x Pinmux 039.xlsx cannot be edited and requires password.
Could you help to provide excel file that can be edited without password?
Thanks
Daniel