Tool/software:
Hi
May I have qustion about AM625x DISPC VP2?
I think this port supporting 24, 18,...-bit parallel display interface.
Question1
If useing 24-bit mode, the LSB is VOUT1_DATA[0]? or VOUT1_DATA[23]?
Question2
If set 24-bit mode, and not use low 6-bit, it be allowed?
Processor side set as 24-bit mode, but Display side use 18-bit.
Question3
If useing 18-bit mode, it may be unconnected DATA[23:18].
Is this mean DATA[23:18] was LSB in 24-bit mode? (signal is same as 24bit mode?)
Or hardware will shift 6-bit such as DATA[23:6](@24-bit mode) shift to DATA[18:0] ?
Thanks,
GR