Other Parts Discussed in Thread: TDA4VL
Tool/software:
Hello, I'm using customed board based tda4vl
And my sdk version is 09_02_00 in j721s2 platform
i use only RTOS mode
Currently, when I connect the lan line to the board, the ethernet connection from the board is not working.
So I have a few questions
1. Is ethernet connection possible on j721s2 platform.
2. Is it possible to enable ethernet in RTOS only mode.
3. If possible, which part should be checked in the current state
root@j721s2-evm:/opt/vision_apps# ./vision_apps_init.sh root@j721s2-evm:/opt/vision_apps# [MCU2_0] 4.514377 s: CIO: Init ... Done !!! [MCU2_0] 4.514429 s: ### CPU Frequency = 1000000000 Hz [MCU2_0] 4.514452 s: CPU is running FreeRTOS [MCU2_0] 4.514469 s: APP: Init ... !!! [MCU2_0] 4.514501 s: SCICLIENT: Init ... !!! [MCU2_0] 4.514615 s: SCICLIENT: DMSC FW version [9.2.4--v09.02.04 (Kool Koala)] [MCU2_0] 4.514641 s: SCICLIENT: DMSC FW revision 0x9 [MCU2_0] 4.514659 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_0] 4.514679 s: SCICLIENT: Init ... Done !!! [MCU2_0] 4.514696 s: UDMA: Init ... !!! [MCU2_0] 4.515523 s: UDMA: Init ... Done !!! [MCU2_0] 4.515552 s: UDMA: Init for CSITX/CSIRX ... !!! [MCU2_0] 4.515975 s: UDMA: Init for CSITX/CSIRX ... Done !!! [MCU2_0] 4.516005 s: MEM: Init ... !!! [MCU2_0] 4.516027 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ b9000000 of size 14680064 bytes !!! [MCU2_0] 4.516068 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 60000000 of size 524288 bytes !!! [MCU2_0] 4.516102 s: MEM: Created heap (DDR_CACHE_WT_MEM, id=7, flags=0x00000000) @ b9e00000 of size 2097152 bytes !!! [MCU2_0] 4.516137 s: MEM: Init ... Done !!! [MCU2_0] 4.516152 s: IPC: Init ... !!! [MCU2_0] 4.516181 s: IPC: 5 CPUs participating in IPC !!! [MCU2_0] 4.516205 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_0] 15.990524 s: IPC: HLOS is ready !!! [MCU2_0] 15.993357 s: IPC: Init ... Done !!! [MCU2_0] 15.993392 s: APP: Syncing with 4 CPUs ... !!! [MCU2_0] 16.109919 s: APP: Syncing with 4 CPUs ... Done !!! [MCU2_0] 16.109946 s: REMOTE_SERVICE: Init ... !!! [MCU2_0] 16.110115 s: REMOTE_SERVICE: Init ... Done !!! [MCU2_0] 16.110145 s: FVID2: Init ... !!! [MCU2_0] 16.110222 s: FVID2: Init ... Done !!! [MCU2_0] 16.110261 s: SCICLIENT: Sciclient_pmSetModuleState module=215 state=2 [MCU2_0] 16.110339 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.110362 s: i2c baseAddr : 40b00000 [MCU2_0] 16.110380 s: i2c baseAddr : 40b00000 [MCU2_0] 16.110397 s: i2c baseAddr : 40b10000 [MCU2_0] 16.110413 s: i2c baseAddr : 40b10000 [MCU2_0] 16.110429 s: i2c baseAddr : 0 [MCU2_0] 16.110444 s: i2c baseAddr : 2000000 [MCU2_0] 16.110460 s: i2c baseAddr : 0 [MCU2_0] 16.110475 s: i2c baseAddr : 2010000 [MCU2_0] 16.110491 s: i2c baseAddr : 0 [MCU2_0] 16.110505 s: i2c baseAddr : 2020000 [MCU2_0] 16.110522 s: i2c baseAddr : 0 [MCU2_0] 16.110537 s: i2c baseAddr : 2030000 [MCU2_0] 16.110553 s: i2c baseAddr : 0 [MCU2_0] 16.110568 s: i2c baseAddr : 2040000 [MCU2_0] 16.110589 s: DSS: Init ... !!! [MCU2_0] 16.110604 s: DSS: Display type is eDP !!! [MCU2_0] 16.110622 s: DSS: M2M Path is enabled !!! [MCU2_0] 16.110638 s: DSS: SoC init ... !!! [MCU2_0] 16.110663 s: SCICLIENT: Sciclient_pmSetModuleState module=158 state=0 [MCU2_0] 16.110717 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.110737 s: SCICLIENT: Sciclient_pmSetModuleState module=365 state=2 [MCU2_0] 16.110899 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.110918 s: SCICLIENT: Sciclient_pmSetModuleState module=156 state=2 [MCU2_0] 16.111015 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.111035 s: SCICLIENT: Sciclient_pmSetModuleState module=365 state=2 [MCU2_0] 16.111106 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.111125 s: SCICLIENT: Sciclient_pmSetModuleState module=156 state=2 [MCU2_0] 16.111309 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.111333 s: SCICLIENT: Sciclient_pmSetModuleState module=158 state=0 [MCU2_0] 16.111499 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.111520 s: SCICLIENT: Sciclient_pmSetModuleClkFreq module=158 clk=3 freq=148500000 [MCU2_0] 16.111717 s: SCICLIENT: Sciclient_pmSetModuleClkFreq success [MCU2_0] 16.111738 s: SCICLIENT: Sciclient_pmModuleClkRequest module=158 clk=3 state=2 flag=2 [MCU2_0] 16.111864 s: SCICLIENT: Sciclient_pmModuleClkRequest success [MCU2_0] 16.111885 s: SCICLIENT: Sciclient_pmSetModuleState module=158 state=2 [MCU2_0] 16.112076 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.112096 s: DSS: SoC init ... Done !!! [MCU2_0] 16.112113 s: DSS: Board init ... !!! [MCU2_0] 16.112128 s: DSS: Turning on DP_PWR pin for eDP adapters ... !!! [MCU2_0] 16.611232 s: DSS: Turning on DP_PWR pin for eDP adapters ... Done!!! [MCU2_0] 16.611261 s: DSS: Board init ... Done !!! [MCU2_0] 16.686283 s: DSS: Init ... Done !!! [MCU2_0] 16.686327 s: VHWA: VPAC Init ... !!! [MCU2_0] 16.686348 s: SCICLIENT: Sciclient_pmSetModuleState module=361 state=2 [MCU2_0] 16.686456 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.686478 s: VHWA: LDC Init ... !!! [MCU2_0] 16.688049 s: VHWA: LDC Init ... Done !!! [MCU2_0] 16.688077 s: VHWA: MSC Init ... !!! [MCU2_0] 16.693722 s: VHWA: MSC Init ... Done !!! [MCU2_0] 16.693749 s: VHWA: NF Init ... !!! [MCU2_0] 16.694543 s: VHWA: NF Init ... Done !!! [MCU2_0] 16.694569 s: VHWA: VISS Init ... !!! [MCU2_0] 16.699778 s: VHWA: VISS Init ... Done !!! [MCU2_0] 16.699817 s: VHWA: VPAC Init ... Done !!! [MCU2_0] 16.699848 s: VX_ZONE_INIT:Enabled [MCU2_0] 16.699866 s: VX_ZONE_ERROR:Enabled [MCU2_0] 16.699883 s: VX_ZONE_WARNING:Enabled [MCU2_0] 16.700993 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target MCU2-0 [MCU2_0] 16.701080 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target VPAC_NF [MCU2_0] 16.701153 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target VPAC_LDC1 [MCU2_0] 16.701240 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target VPAC_MSC1 [MCU2_0] 16.701315 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target VPAC_MSC2 [MCU2_0] 16.701427 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target VPAC_VISS1 [MCU2_0] 16.701510 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CAPTURE1 [MCU2_0] 16.701595 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CAPTURE2 [MCU2_0] 16.701686 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CAPTURE3 [MCU2_0] 16.701768 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CAPTURE4 [MCU2_0] 16.701847 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CAPTURE5 [MCU2_0] 16.701930 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CAPTURE6 [MCU2_0] 16.702017 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CAPTURE7 [MCU2_0] 16.702098 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CAPTURE8 [MCU2_0] 16.702177 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DISPLAY1 [MCU2_0] 16.702264 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DISPLAY2 [MCU2_0] 16.702353 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CSITX [MCU2_0] 16.702430 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target CSITX2 [MCU2_0] 16.702503 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSS_M2M1 [MCU2_0] 16.702586 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSS_M2M2 [MCU2_0] 16.702660 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSS_M2M3 [MCU2_0] 16.702734 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSS_M2M4 [MCU2_0] 16.702765 s: VX_ZONE_INIT:[tivxInitLocal:136] Initialization Done !!! [MCU2_0] 16.702789 s: APP: OpenVX Target kernel init ... !!! [MCU2_0] 16.709382 s: APP: OpenVX Target kernel init ... Done !!! [MCU2_0] 16.709416 s: CSI2RX: Init ... !!! [MCU2_0] 16.709431 s: SCICLIENT: Sciclient_pmSetModuleState module=136 state=2 [MCU2_0] 16.709491 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.709514 s: SCICLIENT: Sciclient_pmSetModuleState module=38 state=2 [MCU2_0] 16.709595 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.709615 s: SCICLIENT: Sciclient_pmSetModuleState module=39 state=2 [MCU2_0] 16.709685 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.709705 s: SCICLIENT: Sciclient_pmSetModuleState module=152 state=2 [MCU2_0] 16.709762 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.709782 s: SCICLIENT: Sciclient_pmSetModuleState module=153 state=2 [MCU2_0] 16.709834 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.709958 s: CSI2RX: Init ... Done !!! [MCU2_0] 16.709979 s: CSI2TX: Init ... !!! [MCU2_0] 16.709994 s: SCICLIENT: Sciclient_pmSetModuleState module=136 state=2 [MCU2_0] 16.710043 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.710063 s: SCICLIENT: Sciclient_pmSetModuleState module=40 state=2 [MCU2_0] 16.710124 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.710144 s: SCICLIENT: Sciclient_pmSetModuleState module=41 state=2 [MCU2_0] 16.710207 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.710234 s: SCICLIENT: Sciclient_pmSetModuleState module=363 state=2 [MCU2_0] 16.710283 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.710304 s: SCICLIENT: Sciclient_pmSetModuleState module=364 state=2 [MCU2_0] 16.710361 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 16.710421 s: CSI2TX: Init ... Done !!! [MCU2_0] 16.710443 s: ISS: Init ... !!! [MCU2_0] 16.710463 s: Found sensor IMX390C_RAW12 at location 0 [MCU2_0] 16.710488 s: IssSensor_Init ... Done !!! [MCU2_0] 16.710538 s: IttRemoteServer_Init ... Done !!! [MCU2_0] 16.710555 s: ISS: Init ... Done !!! [MCU2_0] 16.710572 s: VISS REMOTE SERVICE: Init ... !!! [MCU2_0] 16.710616 s: VISS REMOTE SERVICE: Init ... Done !!! [MCU2_0] 16.710636 s: UDMA Copy: Init ... !!! [MCU2_0] 16.711477 s: UDMA Copy: Init ... Done !!! [MCU2_0] 16.711508 s: APP: Init ... Done !!! [MCU2_0] 16.711527 s: APP: Run ... !!! [MCU2_0] 16.711542 s: IPC: Starting echo test ... [MCU2_0] 16.711649 s: APP: Run ... Done !!! [MCU2_0] 16.712249 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] C7X_1[P] C7X_2[.] [MCU2_0] 16.712304 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] C7X_1[P] C7X_2[P] [MCU2_0] 16.712345 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C7X_1[P] C7X_2[P] [MCU2_1] 4.554042 s: CIO: Init ... Done !!! [MCU2_1] 4.554093 s: ### CPU Frequency = 1000000000 Hz [MCU2_1] 4.554117 s: CPU is running FreeRTOS [MCU2_1] 4.554133 s: APP: Init ... !!! [MCU2_1] 4.554164 s: SCICLIENT: Init ... !!! [MCU2_1] 4.554273 s: SCICLIENT: DMSC FW version [9.2.4--v09.02.04 (Kool Koala)] [MCU2_1] 4.554301 s: SCICLIENT: DMSC FW revision 0x9 [MCU2_1] 4.554320 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_1] 4.554339 s: SCICLIENT: Init ... Done !!! [MCU2_1] 4.554356 s: UDMA: Init ... !!! [MCU2_1] 4.555188 s: UDMA: Init ... Done !!! [MCU2_1] 4.555213 s: MEM: Init ... !!! [MCU2_1] 4.555235 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ ba000000 of size 16777216 bytes !!! [MCU2_1] 4.555275 s: MEM: Init ... Done !!! [MCU2_1] 4.555290 s: IPC: Init ... !!! [MCU2_1] 4.555322 s: IPC: 5 CPUs participating in IPC !!! [MCU2_1] 4.555347 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_1] 16.107060 s: IPC: HLOS is ready !!! [MCU2_1] 16.109865 s: IPC: Init ... Done !!! [MCU2_1] 16.109893 s: APP: Syncing with 4 CPUs ... !!! [MCU2_1] 16.109922 s: APP: Syncing with 4 CPUs ... Done !!! [MCU2_1] 16.109942 s: REMOTE_SERVICE: Init ... !!! [MCU2_1] 16.110121 s: REMOTE_SERVICE: Init ... Done !!! [MCU2_1] 16.110151 s: FVID2: Init ... !!! [MCU2_1] 16.110225 s: FVID2: Init ... Done !!! [MCU2_1] 16.110259 s: VHWA: DMPAC: Init ... !!! [MCU2_1] 16.110276 s: SCICLIENT: Sciclient_pmSetModuleState module=58 state=2 [MCU2_1] 16.110394 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_1] 16.110418 s: SCICLIENT: Sciclient_pmSetModuleState module=62 state=2 [MCU2_1] 16.110479 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_1] 16.110500 s: VHWA: DOF Init ... !!! [MCU2_1] 16.114194 s: VHWA: DOF Init ... Done !!! [MCU2_1] 16.114227 s: VHWA: SDE Init ... !!! [MCU2_1] 16.115364 s: VHWA: SDE Init ... Done !!! [MCU2_1] 16.115393 s: VHWA: DMPAC: Init ... Done !!! [MCU2_1] 16.115423 s: VX_ZONE_INIT:Enabled [MCU2_1] 16.115440 s: VX_ZONE_ERROR:Enabled [MCU2_1] 16.115456 s: VX_ZONE_WARNING:Enabled [MCU2_1] 16.116573 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target MCU2-1 [MCU2_1] 16.116657 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DMPAC_SDE [MCU2_1] 16.116732 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DMPAC_DOF [MCU2_1] 16.116765 s: VX_ZONE_INIT:[tivxInitLocal:136] Initialization Done !!! [MCU2_1] 16.116788 s: APP: OpenVX Target kernel init ... !!! [MCU2_1] 16.116931 s: APP: OpenVX Target kernel init ... Done !!! [MCU2_1] 16.116957 s: UDMA Copy: Init ... !!! [MCU2_1] 16.117786 s: UDMA Copy: Init ... Done !!! [MCU2_1] 16.117819 s: APP: Init ... Done !!! [MCU2_1] 16.117837 s: APP: Run ... !!! [MCU2_1] 16.117852 s: IPC: Starting echo test ... [MCU2_1] 16.117949 s: APP: Run ... Done !!! [MCU2_1] 16.118351 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C7X_1[P] C7X_2[.] [MCU2_1] 16.118398 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C7X_1[P] C7X_2[P] [MCU2_1] 16.712141 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[s] C7X_1[P] C7X_2[P] [C7x_1 ] 4.955987 s: CIO: Init ... Done !!! [C7x_1 ] 4.956004 s: ### CPU Frequency = 1000000000 Hz [C7x_1 ] 4.956016 s: CPU is running FreeRTOS [C7x_1 ] 4.956026 s: APP: Init ... !!! [C7x_1 ] 4.956033 s: SCICLIENT: Init ... !!! [C7x_1 ] 4.956135 s: SCICLIENT: DMSC FW version [9.2.4--v09.02.04 (Kool Koala)] [C7x_1 ] 4.956150 s: SCICLIENT: DMSC FW revision 0x9 [C7x_1 ] 4.956160 s: SCICLIENT: DMSC FW ABI revision 3.1 [C7x_1 ] 4.956171 s: SCICLIENT: Init ... Done !!! [C7x_1 ] 4.956181 s: UDMA: Init ... !!! [C7x_1 ] 4.956942 s: UDMA: Init ... Done !!! [C7x_1 ] 4.956956 s: MEM: Init ... !!! [C7x_1 ] 4.956968 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ 117000000 of size 268435456 bytes !!! [C7x_1 ] 4.956990 s: MEM: Init ... Done !!! [C7x_1 ] 4.956998 s: IPC: Init ... !!! [C7x_1 ] 4.957014 s: IPC: 5 CPUs participating in IPC !!! [C7x_1 ] 4.957028 s: IPC: Waiting for HLOS to be ready ... !!! [C7x_1 ] 13.296364 s: IPC: HLOS is ready !!! [C7x_1 ] 13.297858 s: IPC: Init ... Done !!! [C7x_1 ] 13.297874 s: APP: Syncing with 4 CPUs ... !!! [C7x_1 ] 16.109921 s: APP: Syncing with 4 CPUs ... Done !!! [C7x_1 ] 16.109939 s: REMOTE_SERVICE: Init ... !!! [C7x_1 ] 16.110096 s: REMOTE_SERVICE: Init ... Done !!! [C7x_1 ] 16.110116 s: VX_ZONE_INIT:Enabled [C7x_1 ] 16.110128 s: VX_ZONE_ERROR:Enabled [C7x_1 ] 16.110138 s: VX_ZONE_WARNING:Enabled [C7x_1 ] 16.110359 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP_C7-1 [C7x_1 ] 16.110431 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP_C7-1_PRI_2 [C7x_1 ] 16.110502 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP_C7-1_PRI_3 [C7x_1 ] 16.110576 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP_C7-1_PRI_4 [C7x_1 ] 16.110645 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP_C7-1_PRI_5 [C7x_1 ] 16.110735 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP_C7-1_PRI_6 [C7x_1 ] 16.110805 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP_C7-1_PRI_7 [C7x_1 ] 16.110873 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP_C7-1_PRI_8 [C7x_1 ] 16.110897 s: VX_ZONE_INIT:[tivxInitLocal:136] Initialization Done !!! [C7x_1 ] 16.110918 s: APP: OpenVX Target kernel init ... !!! [C7x_1 ] 16.111079 s: APP: OpenVX Target kernel init ... Done !!! [C7x_1 ] 16.111093 s: APP: Init ... Done !!! [C7x_1 ] 16.111102 s: APP: Run ... !!! [C7x_1 ] 16.111112 s: IPC: Starting echo test ... [C7x_1 ] 16.111193 s: APP: Run ... Done !!! [C7x_1 ] 16.112606 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C7X_1[s] C7X_2[P] [C7x_1 ] 16.118346 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C7X_1[s] C7X_2[P] [C7x_1 ] 16.712156 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C7X_1[s] C7X_2[P] [C7x_2 ] 5.051492 s: CIO: Init ... Done !!! [C7x_2 ] 5.051507 s: ### CPU Frequency = 1000000000 Hz [C7x_2 ] 5.051519 s: CPU is running FreeRTOS [C7x_2 ] 5.051528 s: APP: Init ... !!! [C7x_2 ] 5.051535 s: SCICLIENT: Init ... !!! [C7x_2 ] 5.051636 s: SCICLIENT: DMSC FW version [9.2.4--v09.02.04 (Kool Koala)] [C7x_2 ] 5.051650 s: SCICLIENT: DMSC FW revision 0x9 [C7x_2 ] 5.051661 s: SCICLIENT: DMSC FW ABI revision 3.1 [C7x_2 ] 5.051672 s: SCICLIENT: Init ... Done !!! [C7x_2 ] 5.051682 s: UDMA: Init ... !!! [C7x_2 ] 5.052458 s: UDMA: Init ... Done !!! [C7x_2 ] 5.052472 s: MEM: Init ... !!! [C7x_2 ] 5.052483 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ 127000000 of size 16777216 bytes !!! [C7x_2 ] 5.052505 s: MEM: Init ... Done !!! [C7x_2 ] 5.052514 s: IPC: Init ... !!! [C7x_2 ] 5.052530 s: IPC: 5 CPUs participating in IPC !!! [C7x_2 ] 5.052546 s: IPC: Waiting for HLOS to be ready ... !!! [C7x_2 ] 13.602804 s: IPC: HLOS is ready !!! [C7x_2 ] 13.604177 s: IPC: Init ... Done !!! [C7x_2 ] 13.604192 s: APP: Syncing with 4 CPUs ... !!! [C7x_2 ] 16.109921 s: APP: Syncing with 4 CPUs ... Done !!! [C7x_2 ] 16.109938 s: REMOTE_SERVICE: Init ... !!! [C7x_2 ] 16.110098 s: REMOTE_SERVICE: Init ... Done !!! [C7x_2 ] 16.110119 s: VX_ZONE_INIT:Enabled [C7x_2 ] 16.110130 s: VX_ZONE_ERROR:Enabled [C7x_2 ] 16.110141 s: VX_ZONE_WARNING:Enabled [C7x_2 ] 16.110741 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:116] Added target DSP-1 [C7x_2 ] 16.110763 s: VX_ZONE_INIT:[tivxInitLocal:136] Initialization Done !!! [C7x_2 ] 16.110776 s: APP: OpenVX Target kernel init ... !!! [C7x_2 ] 16.111088 s: APP: OpenVX Target kernel init ... Done !!! [C7x_2 ] 16.111102 s: UDMA Copy: Init ... !!! [C7x_2 ] 16.112239 s: UDMA Copy: Init ... Done !!! [C7x_2 ] 16.112253 s: APP: Init ... Done !!! [C7x_2 ] 16.112263 s: APP: Run ... !!! [C7x_2 ] 16.112271 s: IPC: Starting echo test ... [C7x_2 ] 16.112354 s: APP: Run ... Done !!! [C7x_2 ] 16.112612 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C7X_1[P] C7X_2[s] [C7x_2 ] 16.118355 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C7X_1[P] C7X_2[s] [C7x_2 ] 16.712165 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C7X_1[P] C7X_2[s] root@j721s2-evm:/opt/vision_apps# root@j721s2-evm:/opt/vision_apps# root@j721s2-evm:/opt/vision_apps# ifconfig eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500 inet6 fe80::9a03:8aff:fe6e:f2d7 prefixlen 64 scopeid 0x20<link> ether 98:03:8a:6e:f2:d7 txqueuelen 1000 (Ethernet) RX packets 0 bytes 0 (0.0 B) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 22 bytes 3424 (3.3 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536 inet 127.0.0.1 netmask 255.0.0.0 inet6 ::1 prefixlen 128 scopeid 0x10<host> loop txqueuelen 1000 (Local Loopback) RX packets 92 bytes 7654 (7.4 KiB) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 92 bytes 7654 (7.4 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
it's my log Thank you.