This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: how to run yolov8/v11 in this board

Part Number: SK-AM62A-LP
Other Parts Discussed in Thread: TDA4VM

Tool/software:

hello,i referenced edgeai-tidl-tools/docs/custom_model_evaluation.md at master · TexasInstruments/edgeai-tidl-tools · GitHub   edgeai-tidl-tools/examples/osrt_python/README.md at master · TexasInstruments/edgeai-tidl-tools · GitHub

compile in x86 pc

i tried to add new  arguments  in     edgeai-tidl-tools/examples/orst_python/model_configs.py

models_configs = {
############ onnx models ##########
'yolov8n-ori' : {
'model_path' : os.path.join(models_base_path, 'yolov8n.onnx'),
'mean': [0, 0, 0],
'scale' : [0,0,0],
'num_images' : numImages,
'num_classes': 80,
'model_type': 'detection',

#'od_type' : 'YoloV',
'session_name' : 'onnxrt' ,
'framework' : ''
},

}

edgeai-tidl-tools/examples/orst_python/ort/onnxrt_ep.py的

models = [
#"cl-ort-resnet18-v1",
# "od-ort-ssd-lite_mobilenetv2_fpn"
'yolov8n-ori'
]

Here's the error:

====================================================================================================

Command : python3 tflrt_delegate.py in Dir : examples/osrt_python/tfl Started
Running 0 Models - []

Command : python3 onnxrt_ep.py in Dir : examples/osrt_python/ort Started
Available execution providers : ['TIDLExecutionProvider', 'TIDLCompilationProvider', 'CPUExecutionProvider']

Running 1 Models - ['yolov8n-ori']

Process Process-1:
Traceback (most recent call last):
File "/home/zxb/.pyenv/versions/3.10.15/lib/python3.10/multiprocessing/process.py", line 314, in _bootstrap
self.run()
File "/home/zxb/.pyenv/versions/3.10.15/lib/python3.10/multiprocessing/process.py", line 108, in run
self._target(*self._args, **self._kwargs)
File "/home/zxb/Desktop/ti/edgeai-tidl-tools/examples/osrt_python/ort/onnxrt_ep.py", line 221, in run_model
download_model(models_configs, model)
File "/home/zxb/Desktop/ti/edgeai-tidl-tools/examples/osrt_python/common_utils.py", line 240, in download_model
model_path = models_configs[model_name]["session"]["model_path"]
KeyError: 'session'

Running_Model : yolov8n-ori

============================================================================================================================

can i  trouble ti  to give some examples of yolov8,thanks

  • Hello,

    It looks like the current error is that it is not finding your model file "yolov8n.onnx'", so it is trying to download the model and not finding the right model_config information. 

    Which commit / tag are you using for edgeai-tidl-tools? The format of model_configs.py changed from release tag 10_00_06_00 to 10_00_08_00. I see you are using a model config in the 10_00_06 style

    Where did you source your YOLOV8 from? This model is handled abnormally because the original implementation has an unfriendly license such that we cannot post any versions of it. We also require some modifications to the original architecture for it to accelerate well on our AI accelerator (C7xMMA). We offer some guidance on how to get a TI-lite / C7x-MMA friendly version. Please see here: https://github.com/TexasInstruments/edgeai-tensorlab/issues/7.

    • This does mean that I don't have any examples that can be directly shared due to licensing restrictions on YOLOv8
  • Hello,

    i followed u advice to use edgeai-optimization,when using PTC example ,FX Graph Mode Quantization is in maintenance mode.

    Since it is our first time facing this type of model deployment which uses artifacts,can u give some advice or  steps suggestion.

    Our previous projects all used YOLOV8.Should i use  trained v8model to optimization (PTQ /QAT PTC).Or use edgeai-yolox/edgeai-mmdetetion to retrain a new v8-ti-lite model offline ,since our company's dataset doesn’t allow any uploading.

    I use modelmaker running    ./run_modelmaker.sh AM62A config_detection.yaml  but failed. Here are the logs.Pray for your valuable advice and detailed step-by-step instructions

    modelmaker-log.txtmodeloptimization-PTC-log.txt

  • If there is any other ways to use MPU or DSP  

  • Hello,

    I understand -- I know this process can be confusing on the first attempt. I'll help however I can! I will respond to a few parts of your last comment. Please note that this is not an ordered list of steps

    A) general suggestion

    My first suggestion is to follow one of the examples in edgeai-tidl-tools and the custom-model workflow. Take one of our existing models like yolox (pretrained), and see how the examples/osrt_python/ort/onnxrt_ep.py is used to compile and run the model on the host. You can follow the steps in the README to transfer portions of edgeai-tidl-tools (examples, test_data, models, model-artifacts) to the EVM and run the model on static input. 

    • I recommend this not because it solves your problem. I recommend this so you can learn the development flow on a known working model, since your yolov8 will add more complexity.
      • I'll address your model in part D of the response.

    B) PTC logs

    Your jupyter notebook look like they are using an outdated repository. We migrated several months ago from multiple edgeai- repos for model training and development, and wrapped those into the edgeai-tensorlab repo to make repo-versioning more consistent and controlled. You can continue using these repos if you are intentionally targeting an older SDK version like 9.1, but otherwise I suggest cloning edgeai-tensorlab and working from that repository instead.

    I see you modelmaker log mentions you are targeting 9.1 SDK. The modeloptimization tooling was fairly new at this point, and I'm less confident about this version that more recent releases (r9.2 and r10.0 corresponding to SDK versions). 

    • I also see setup errors for scipy due to a BLAS/LAPACK dependency. This probably requires a system-level package that cannot be installed by pip3. I'd recommend searching with google for guidance here. 

    C) Modelmaker logs

    Looks like modelmaker trained the model but failed to compile. This means that pytorch trained yolox and produced an ONNX file. The next stage is compilation, which uses edgeai-benchmark -- this is an alternative to edgeai-tidl-tools.

    • edgeai-benchmark is for testing/compiling with larger datasets. It can compile the model and then test the accuracy of that model on your dataset
      • typically used by advanced users or as part of modelmaker workflow
    • edgeai-tidl-tools is for baseline evaluation of inference speed and accuracy on a smaller set of data. 
        • typically used for initial testing on new models. Often, this is sufficient for compiling model artifacts and testing 

      Your model failed during edgeai-benchmark compilation because it could not find a dependency: 


      ImportError: cannot import name 'onnx_model_opt' from 'osrt_model_tools.onnx_tools' (/home/zxb/.pyenv/versions/py310/lib/python3.10/site-packages/osrt_model_tools/onnx_tools/__init__.py)

      This dependency is setup as part of edgeai-tidl-tools, and the source python is under the /scripts directory (osrt_model_tools/onnx_tools). The imported function is meant to add some preprocessing layers to the model (YOLOX) that will allow uint8 input instead of float. This is why a later error complained about this input data type

      • What is the commit tag / branch of edgeai-tidl-tools? It may have setup a more recent version. The appropriate release would be 09_01_07_00We should be able to update with the proper tools and rerun this
        • alteratively, take the trained ONNX model and import using edgeai-tidl-tools standalone. This is related to suggestion A

      i followed u advice to use edgeai-optimization,when using PTC example ,FX Graph Mode Quantization is in maintenance mode.

      Could you explain more, please? I assume you mean that you followed the steps for modifying the yolov8 model based on the linked issue in edgeai-tensorlab repo. I'm not sure what you mean by "FX Graph Mode Quantization is in maintenance mode"

      D) YOLOv8 Guidance

      The steps detailed in that issue-7 explain how to train a modified yolov8 that will work well with TI's accelerator (C7xMMA). This training flow uses the upstream mmyolo repo, which is patched with files on that tensorlab issue-7 that will modify model structure to be better for C7xMMA. This does require some retraining.

      Since you have a pretrained model, you can use those weights as the starting point for retraining this modified structure. It should not take more than 100 epochs to retrain this way, but depending on your yolov8 source, it could take effort to get the pretrained weights aligned with the most appropriate yolov8-config The PTH for your yolov8 would need to have tensor/weights named similarly to what the mmyolo repo's yolov8 versions expect. 

      Our previous projects all used YOLOV8.Should i use  trained v8model to optimization (PTQ /QAT PTC).Or use edgeai-yolox/edgeai-mmdetetion to retrain a new v8-ti-lite model offline ,since our company's dataset doesn’t allow any uploading.

      I would encourage the first option here --

      1. use your trained model with a patched version of mmyolo to apply our model surgery
      2. retrain for 25-100 epochs at low learning rate.
        1. You may also run QAT at this time if you wish. I would suggest not on the first attempt. You may come back and do this later if accuracy from PTQ is not sufficient.
      3. Export the model to ONNX format with an accompanying prototxt file that describes the detection head.
      4. Use this ONNX and PROTOTXT to import/compile the model with edgeai-tidl-tools/examples/osrt_python/ort/onnxrt_ep.py.
        1. Follow the custom-model guidelines in that repo 
        2. this will produce artifacts

      BR,
      Reese

    • Hello,

      Yesterday, I found yolov8_to-mmyolo. py in mmyolo/tools/model_comverters, so this morning I tried it out and obtained the mmyolo formatted. pth using yolov8n.pt. Then, I followed the patch version of mmyolo, Python projects/easyplot/tools/export_onnx.py. \ config \ yolov8 \ yolov8_n_cyncbn_fast_8xb16-500e_coco. py. \ myolov8n.psh -- work dir. \ tests \ -- img-size 640 640-- simplify -- iou threshold 0.65-- score threshold 0.25-- opset 12-- backend ONNSRUNTIME. This is the onnx

       ,But it won't generate protoxt files. When there was a Module NotFoundError: there was no module named 'edgeai_torchmodelopt', I copied edgeai-tensorlab-main\edgeai-modeloptimization\torchmodelopt to mmyolo\projects\easydeploy\tools\export_onnx.py and then encountered an ImportError: unable to import the name “_parse_stack_trace”(C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\torch\fx\graph.py).

      This seems to be the result of a conflict between torch2.0.1cu117 and mmcv2.0.1. At present, the MMYOLO patch has added a version conflict issue edgeai_torchmodelopt. MMYOLO only supports mim install "mmcv>=2.0.0rc4,<2.1.0", but mmcv below 2.1.0 only supports CUDA11.7~11.0 TORCH2.0. However, this results in torch.fx.graph not having passwrse_stack_trace for x~1.13. x. I tried installing torch from 2.0.0 to 2.4.0 and found that only torch 2.2. x~passwase_dack_trace was available. Is this a bug github.com/.../7 the last issue seems to be the same with mine.

       

      Here comes the new problems:HOW TO GET THE ONNX AND PROTOTXT MODELS. I tried to use mmyolo and mmdetection both can't use because of the same question github.com/.../7 .If i change torch to 2.4.1 using mmdetetion,it comes with  the problem of mmengine.registry's OPTIMIZERS . yolov8_s_syncbn_fast_8xb16-500e.py can be used in MMYOLO to generate onnx model,but in mmdetetion configs in mmyolo can't be uesd.

      KeyError: 'YOLODetector is not in the model registry. Please check whether the value of `YOLODetector` is correct or it was registered as expected. More details can be found at mmengine.readthedocs.io/.../config.html

      Is there any other way to get onnx and prototxt .

    • Hello,

      Okay, it sounds like you have a trained version such that .PTH weights is available, and you just need ONNX+PROTOTXT to enable import with TIDL tools.  Is your trained PTH weights from before or after edgeai_torchmodelopt calls? 

      We will need to look deeper into this -- I must ask for your patience here. The version incompatibility does indeed look frustrating.

      • Can you provide a list of your packages and versions?
        • If you tried multiple difference dependency configurations, please list those with corresponding versioning.
      • What is the commit ID / release tag for the edgeai-tensorlab repo?
        • The issue-7 was from July, so closest tag is probably r9.2

      BR,
      Reese

    • Hello,

          .PTH is from before  edgeai_torchmodelopt callsSince mmyolo only support mmcv>=2.0.0.rc4~<2.1.0, while mmcv2.0.1 need cuda<=11.7 and torch <=2.0.x,edgeai-modeloptimization needs  torch.fx.graph  which is only supported  torch 2.2.x~2.4.x.I tried lots of  versions matchs of these packages,but all failed. 

      Here is the  list of my packages and versions.

      WARNING: Ignoring invalid distribution -orch (c:\users\admin\.conda\envs\mmyolo\lib\site-packages)
      Package Version
      ---------------------------- ------------
      absl-py 2.1.0
      addict 2.4.0
      aiofiles 23.2.1
      aiohappyeyeballs 2.4.0
      aiohttp 3.10.5
      aiosignal 1.3.1
      albucore 0.0.17
      albumentations 1.4.18
      aliyun-python-sdk-core 2.15.2
      aliyun-python-sdk-kms 2.16.4
      altgraph 0.17.4
      annotated-types 0.7.0
      antlr4-python3-runtime 4.9.3
      anyio 4.4.0
      appdirs 1.4.4
      astunparse 1.6.3
      async-timeout 4.0.3
      attrs 24.2.0
      audioread 3.0.1
      beautifulsoup4 4.12.3
      blinker 1.8.2
      branca 0.7.2
      Brotli 1.1.0
      cachetools 5.5.0
      certifi 2024.7.4
      cffi 1.17.0
      charset-normalizer 3.3.2
      click 8.1.7
      cnocr 2.3.0.3
      cnstd 1.2.4.2
      colorama 0.4.6
      coloredlogs 15.0.1
      contourpy 1.1.1
      crcmod 1.7
      cryptography 43.0.0
      cycler 0.12.1
      Cython 3.0.11
      datasets 2.21.0
      DeepFilterLib 0.5.2
      deepfilternet 0.5.2
      dill 0.3.8
      docker-pycreds 0.4.0
      editdistance 0.8.1
      einops 0.8.0
      eiq 2.2.0
      et-xmlfile 1.1.0
      eval_type_backport 0.2.0
      exceptiongroup 1.2.2
      fastapi 0.112.2
      ffmpy 0.4.0
      filelock 3.14.0
      Flask 3.0.3
      flatbuffers 24.3.25
      folium 0.17.0
      fonttools 4.53.1
      frozenlist 1.4.1
      fsspec 2024.6.1
      funasr 1.0.27
      gast 0.4.0
      gdown 5.2.0
      geographiclib 2.0
      geopy 2.4.1
      gitdb 4.0.11
      GitPython 3.1.43
      google-auth 2.34.0
      google-auth-oauthlib 1.0.0
      google-pasta 0.2.0
      gradio 4.42.0
      gradio_client 1.3.0
      greenlet 3.1.1
      grpcio 1.66.1
      h11 0.14.0
      h2 4.1.0
      h5py 3.11.0
      hpack 4.0.0
      httpcore 1.0.5
      httpx 0.27.2
      huggingface-hub 0.24.6
      humanfriendly 10.0
      hydra-core 1.3.2
      hyperframe 6.0.1
      idna 3.8
      ImageHash 4.3.1
      imageio 2.35.1
      imgviz 1.7.5
      importlib_metadata 8.5.0
      importlib_resources 6.4.4
      itsdangerous 2.2.0
      jaconv 0.4.0
      jamo 0.4.1
      jax 0.4.13
      jieba 0.42.1
      Jinja2 3.1.4
      jmespath 0.10.0
      joblib 1.4.2
      kaldiio 2.18.0
      keras 2.13.1
      kiwisolver 1.4.5
      labelImg 1.8.6
      labelme 5.5.0
      lazy_loader 0.4
      libclang 18.1.1
      librosa 0.10.2
      lightning-utilities 0.11.8
      llvmlite 0.41.1
      loguru 0.7.2
      lxml 5.3.0
      Markdown 3.7
      markdown-it-py 3.0.0
      MarkupSafe 2.1.5
      matplotlib 3.7.5
      mdurl 0.1.2
      mediapipe 0.10.11
      ml-dtypes 0.2.0
      mmcv 2.0.1
      mmdet 3.3.0
      mmengine 0.10.5
      mmyolo 0.6.0
      model-index 0.1.11
      modelscope 1.17.1
      more-itertools 10.4.0
      mpmath 1.3.0
      msgpack 1.0.8
      multidict 6.0.5
      multiprocess 0.70.16
      mysql 0.0.3
      mysql-connector-python 9.0.0
      mysqlclient 2.2.4
      natsort 8.4.0
      networkx 3.1
      numba 0.58.1
      numpy 1.23.5
      oauthlib 3.2.2
      omegaconf 2.3.0
      onnx 1.17.0
      onnxruntime 1.19.0
      onnxsim 0.4.36
      openai-whisper 20231117
      opencv-contrib-python 4.10.0.84
      opencv-python 4.10.0.84
      opencv-python-headless 4.10.0.84
      opendatalab 0.0.10
      openmim 0.3.9
      openpyxl 3.1.5
      openxlab 0.1.2
      opt-einsum 3.3.0
      ordered-set 4.1.0
      orjson 3.10.7
      oss2 2.17.0
      outcome 1.3.0.post0
      packaging 24.2
      pandas 2.0.3
      pefile 2023.2.7
      pillow 10.4.0
      pip 24.3.1
      platformdirs 4.3.6
      Polygon3 3.0.9.1
      pooch 1.8.2
      prettytable 3.11.0
      protobuf 3.20.3
      psutil 6.1.0
      py-cpuinfo 9.0.0
      pyarrow 17.0.0
      pyasn1 0.6.0
      pyasn1_modules 0.4.0
      PyAudio 0.2.14
      pyclipper 1.3.0.post6
      pycocotools 2.0.7
      pycocotools-windows 2.0.0.2
      pycparser 2.22
      pycryptodome 3.20.0
      pydantic 2.8.2
      pydantic_core 2.20.1
      pydub 0.25.1
      Pygments 2.18.0
      pyinstaller 6.11.1
      pyinstaller-hooks-contrib 2024.10
      PyMySQL 1.1.1
      pynndescent 0.5.13
      pyparsing 3.1.4
      PyQt5 5.15.11
      PyQt5-Qt5 5.15.2
      PyQt5_sip 12.15.0
      pyreadline3 3.4.1
      PySocks 1.7.1
      PySoundFile 0.9.0.post1
      pytesseract 0.3.13
      python-dateutil 2.9.0.post0
      python-multipart 0.0.9
      pytorch-wpe 0.0.1
      pytz 2023.4
      PyWavelets 1.4.1
      pywin32 308
      pywin32-ctypes 0.2.3
      PyYAML 6.0.2
      QtPy 2.4.1
      regex 2024.7.24
      requests 2.28.2
      requests-oauthlib 2.0.0
      rich 13.4.2
      rotary-embedding-torch 0.6.5
      rsa 4.9
      ruff 0.6.3
      safetensors 0.4.4
      scikit-image 0.21.0
      scikit-learn 1.3.2
      scipy 1.10.1
      seaborn 0.13.2
      selenium 4.26.1
      semantic-version 2.10.0
      sentencepiece 0.2.0
      sentry-sdk 2.18.0
      setproctitle 1.3.3
      setuptools 60.2.0
      shapely 2.0.6
      shellingham 1.5.4
      simplejson 3.19.3
      six 1.16.0
      smmap 5.0.1
      sniffio 1.3.1
      sortedcontainers 2.4.0
      sounddevice 0.5.0
      soundfile 0.12.1
      soupsieve 2.6
      soxr 0.3.7
      SQLAlchemy 2.0.35
      starlette 0.38.4
      sympy 1.13.2
      tabulate 0.9.0
      tensorboard 2.13.0
      tensorboard-data-server 0.7.2
      tensorboardX 2.6.2.2
      tensorflow 2.13.0
      tensorflow-estimator 2.13.0
      tensorflow-intel 2.13.0
      tensorflow-io-gcs-filesystem 0.31.0
      termcolor 2.4.0
      terminaltables 3.1.10
      Theano 1.0.5
      threadpoolctl 3.5.0
      tifffile 2023.7.10
      tiktoken 0.7.0
      timm 1.0.9
      tomli 2.0.1
      tomlkit 0.12.0
      torch 1.13.0+cu117
      torchaudio 0.13.0+cu117
      torchinfo 1.8.0
      torchmetrics 1.5.2
      torchvision 0.14.0+cu117
      tqdm 4.65.2
      trio 0.27.0
      trio-websocket 0.11.1
      ttach 0.0.3
      typer 0.12.5
      typing_extensions 4.12.2
      tzdata 2024.1
      ultralytics 8.2.85
      ultralytics-thop 2.0.11
      umap-learn 0.5.6
      Unidecode 1.3.8
      urllib3 1.26.20
      uvicorn 0.30.6
      wandb 0.18.6
      wcwidth 0.2.13
      websocket-client 1.8.0
      websockets 12.0
      Werkzeug 3.0.4
      wheel 0.45.1
      win_inet_pton 1.1.0
      win32-setctime 1.1.0
      wrapt 1.16.0
      wsproto 1.2.0
      xlrd 2.0.1
      xlutils 2.0.0
      xlwt 1.3.0
      xxhash 3.5.0
      xyzservices 2024.6.0
      yapf 0.40.2
      yarl 1.9.4
      zipp 3.20.2
      zstandard 0.23.0
      (mmyolo) PS D:\zxb\accc\mmyolo> 

      Then i tried edgeai-mmdetection,it can use edgeai-modeloptimization,but it comes with the problems of configs.I tried to copy configs from mmyolo/config/yolov8/    but some module are not supported need to use mmengine registe custom module

      Also,i tried edgeai-modelmaker     ./run_modelmaker.sh   AM62A   ./config_detection.yaml   ,afer i resolved other problems. It  ended with FileNotFoundError: [Errno 2] No such file or directory: '/home/zxb/Desktop/ti/edgeai-modelmaker/data/projects/tiscapes2017_driving/run/20241203-142720/yolox_nano_lite/compilation/AM62A/pkg/artifacts.yaml'.Under the same folder the model is optimized ,but artifacts folder is empty.

      modelmaker-trainlog.txt
      Fullscreen
      1
      2
      3
      4
      5
      6
      7
      8
      9
      10
      11
      12
      13
      14
      15
      16
      17
      18
      19
      2024-12-03 14:28:39,693 - mmdet - INFO - Exp name: yolox_nano_lite.py
      2024-12-03 14:28:39,693 - mmdet - INFO - Epoch(val) [1][107] bbox_mAP: 0.1130, bbox_mAP_50: 0.2410, bbox_mAP_75: 0.0960, bbox_mAP_s: 0.0020, bbox_mAP_m: 0.0940, bbox_mAP_l: 0.4320, bbox_mAP_copypaste: 0.113 0.241 0.096 0.002 0.094 0.432
      /home/zxb/.pyenv/versions/py310/lib/python3.10/site-packages/mmcv/onnx/info.py:20: UserWarning: DeprecationWarning: This function will be deprecated in future. Welcome to use the unified model deployment toolbox MMDeploy: https://github.com/open-mmlab/mmdeploy
      warnings.warn(msg)
      /home/zxb/.pyenv/versions/py310/lib/python3.10/site-packages/mmcv/tensorrt/init_plugins.py:51: UserWarning: DeprecationWarning: This function will be deprecated in future. Welcome to use the unified model deployment toolbox MMDeploy: https://github.com/open-mmlab/mmdeploy
      warnings.warn(msg)
      /home/zxb/.pyenv/versions/py310/lib/python3.10/site-packages/torch/onnx/symbolic_opset9.py:1248: UserWarning: This model contains a squeeze operation on dimension 1. If the model is intended to be used with dynamic input shapes, please use opset version 11 to export the model.
      warnings.warn(
      ============== Diagnostic Run torch.onnx.export version 2.0.1+cpu ==============
      verbose: False, log level: Level.ERROR
      ======================= 0 NONE 0 NOTE 0 WARNING 0 ERROR ========================
      Successfully exported ONNX model: /home/zxb/Desktop/ti/edgeai-modelmaker/data/projects/tiscapes2017_driving/run/20241203-142720/yolox_nano_lite/training/model.onnx
      Trained model is at: /home/zxb/Desktop/ti/edgeai-modelmaker/data/projects/tiscapes2017_driving/run/20241203-142720/yolox_nano_lite/training
      SUCCESS: ModelMaker - Training completed.
      INFO:20241203-142844: model import is in progress - please see the log file for status.
      configs to run: ['od-8200']
      XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    • Thank you for supplying this. What is the commit ID for mmyolo repo? It is supposed to be 8c4d9dc503dc8e327bec8147e8dc97124052f693 to match issue-7.  I agree that the dependencies as you've shown them are incompatible. There may be other 

      Using the mmdetection from our edgeai-modelmaker is a different topic, and I would recommend looking at this in a separate thread. It is difficult to track multiple topics that are so similar in the same thread -- I am concerned it will cause additional confusion. Can you make a separate e2e thread for training/compiling yolox model?

      • looks like training finished and compilation failed to start
      • In the new thread, please show the configuration file passed to model maker and show the directory structure/tree for that  /home/zxb/Desktop/ti/edgeai-modelmaker/data/projects/tiscapes2017_driving/run/20241203-142720/yolox_nano_lite/
        • Note the date string will change if you rerun this. I am interested what is under the training and compilation directories. 

      BR,
      Reese

    • Hello,

             This is different pyenv and different projects with different problems.Considering it is still in the evaluation stage,we are trying to use our v8 models to deploy DMS/OMS in AM62A which will be used in car.So we  maked two plans.

              Plan A using v8 model  and convert it to mmyolov8-lite ,but failed with above environment problems to get onnx and prototxt which will be used to compose.
      mmyolo:commit 8c4d9dc503dc8e327bec8147e8dc97124052f693 (HEAD, tag: v0.6.0, origin/main, origin/HEAD, main)

      mmdetection:commit 7146beba638862b5df251bc248524cfcd8338c9b (HEAD -> r9.1, origin/r9.1, origin/main, origin/HEAD)

      edgeai-modelmaker: commit b4e9b7fda9b9d3ee0f8190bdb49792e001d60e8f (HEAD -> main, origin/r9.1, origin/main, origin/HEAD)

      edgeai-tidl-tools: commit efae61031b31aa2ba5491c03bb808216d3baef14 (HEAD -> master, tag: 10_00_08_00, origin/rel_10_00, origin/master, origin/HEAD)

              Plan B is try to use modelmaker ,using yolox example ,but failed with above log problems ,in this case we just  change the yaml's   train- epoch=1..   /run_modelmaker.sh AM62A ./config_detection.yaml            

      config_detection.yaml :

      ====================================================================================
      common:
      target_module: 'vision'
      task_type: 'detection'
      target_device: 'TDA4VM'
      # run_name can be any string, but there are some special cases:
      # {date-time} will be replaced with datetime.datetime.now().strftime("%Y%m%d-%H%M%S")
      # {model_name} will be replaced with the name of the model
      run_name: '{date-time}/{model_name}'

      dataset:
      # enable/disable dataset loading
      enable: True #False
      # max_num_files: [750, 250] #None

      # Object Detection Dataset Examples:
      # -------------------------------------
      # Example 1, (known datasets): 'widerface_detection', 'pascal_voc0712', 'coco_detection', 'udacity_selfdriving', 'tomato_detection', 'tiscapes2017_driving'
      # dataset_name: widerface_detection
      # -------------------------------------
      # Example 2, give a dataset name and input_data_path.
      # input_data_path could be a path to zip file, tar file, folder OR http, https link to zip or tar files
      # for input_data_path these are provided with this repository as examples:
      # 'software-dl.ti.com/.../tiscapes2017_driving.zip'
      # 'software-dl.ti.com/.../animal_detection.zip'
      # -------------------------------------
      # Example 3, give image folders with annotation files (require list with values for both train and val splits)
      # dataset_name: coco_detection
      # input_data_path: ["./data/projects/coco_detection/dataset/train2017",
      # "./data/projects/coco_detection/dataset/val2017"]
      # input_annotation_path: ["./data/projects/coco_detection/dataset/annotations/instances_train2017.json",
      # "./data/projects/coco_detection/dataset/annotations/instances_val2017.json"]
      # -------------------------------------
      dataset_name: tiscapes2017_driving
      input_data_path: 'software-dl.ti.com/.../tiscapes2017_driving.zip'

      training:
      # enable/disable training
      enable: True #False

      # Object Detection model chosen can be changed here if needed
      # options are: 'yolox_s_lite', 'yolox_tiny_lite', 'yolox_nano_lite', 'yolox_pico_lite', 'yolox_femto_lite'
      model_name: 'yolox_nano_lite'

      training_epochs: 1 #30
      # batch_size: 8 #32
      # learning_rate: 0.005
      # num_gpus: 0 #1 #4

      compilation:
      # enable/disable compilation
      enable: True #False
      # tensor_bits: 8 #16 #32

      =====================================================================================2818.modelmaker-trainlog.txt

    • Hello,

      Understood, option A would be preferred, I presume. 

      mmyolo:commit 8c4d9dc503dc8e327bec8147e8dc97124052f693 (HEAD, tag: v0.6.0, origin/main, origin/HEAD, main)

      mmdetection:commit 7146beba638862b5df251bc248524cfcd8338c9b (HEAD -> r9.1, origin/r9.1, origin/main, origin/HEAD)

      edgeai-modelmaker: commit b4e9b7fda9b9d3ee0f8190bdb49792e001d60e8f (HEAD -> main, origin/r9.1, origin/main, origin/HEAD)

      edgeai-tidl-tools: commit efae61031b31aa2ba5491c03bb808216d3baef14 (HEAD -> master, tag: 10_00_08_00, origin/rel_10_00, origin/master, origin/HEAD)

      Thank you for including, this is helpful.

      Edgeai-modelmaker repository has been moved into the edgeai-tensorlab repo. Please use edgeai-tensorlab repository instead of edgeai-modelmaker, since the latter has been archived. The same is true of edgeai-mmdetection. Please setup the edgeai-tensorlab repo to replace these -- I would recommend using a virtual environment to keep dependencies separate. I believe you have the archived versions of modelmaker and mmdetection repos installed. Edgeai-tensorlab will include a version of those two archived repos that have been version controlled against each other. 

      Your mmyolo version should be okay. When you setup edgeai-tensorlab, I would recommend using the r9.2 branch/tag. I see from git-blames that r10.0 introduces this versioning issue within edgeai-tensorlab/edgeai-modeloptimization, whereas 9.2 does not include this. The following dependencies are expected to work for this r9.2 branch + upstream mmyolo

      torch==2.0.1 torchvision==0.15.2 torchaudio==2.0.2

      Regarding option B

      In your screenshot, I see that a model.onnx and model.prototxt are present. Do these files look normal, e.g. can you load .ONNX in Netron and does prototxt look similar to the one here? 

      Compilation may have failed, but training completed and should have produced the trained model. The error above about failing to open artifacts.yaml is most likely because the path there was not created (MODEL_DIR/AM62A/compilation/pkg). Is that 'artifacts' directory empty under AM62A/compilation/work/od-8200/artifacts?

    • Hello,

         i found that  github.com/.../7   there is a latest solution.So i tried  mmyolov8 and yolov5s6_640_ti_lite_37p4_56p0.onnx. And use edgeai-benchmark get the  yolov5s6_640_ti_lite_37p4_56p0's   artifacts,but the onnx model in artifacts/model  input (fp32) output(32).

      But when i try to run it but failed. Your  FAE told me to git edgeai-dl-tools and run ./setup_target_device.sh ,but this just comes with new problems with py3.12.How run these artifacts. We need your valuable advice

         imagedet-7_onnxrt_Desktop_ti_yolov5s6_640_ti_lite_37p4_56p0_onnx.tar

    • Hi 

      It seems that you are using sdk 10.0. Can you make sure the benchmark is rc10.0 too?

      Regards,

      Adam

    • Hello,

      Echoing what Adam has said -- please check that the benchmark tools are also on r10.0

      In the second image, you run this onnx_inference.py and see a message about 

      "ERROR: Config file size (37912 bytes) does not match size of sTIDL_IOBufDesc_t (94616bytes)"

      The config file size is a _tidl_io_1.bin file's size in bytes and the sTIDL_IOBufDesc_t  is a struct that that file's data will fit into. These sizes are directly related to the SDK version. 

      This tells me that your compiled artifacts are for an older SDK than the one you are running. 37912 bytes corresponds to SDK 9.1 and 94616 correspond to SDK 10.0. 

       

      Your model needs to compiled against the 10.0 tidl_tools to work with the 10.0 SDK. 

      • tidl_tools.tar.gz is generally downloaded while running a setup script. It downloads the tarball from a URL like: 
        • https://software-dl.ti.com/jacinto7/esd/tidl-tools/10_00_08_00/TIDL_TOOLS/AM62A/tidl_tools.tar.gz
          • where 10_00_08_00 is a version string
      •  ./setup_target_device.sh is probably not helpful here -- this is intended for updating the ONNXRuntime, Tensorflow Lite and TVM, and firmware on an SDK like 9.2 that wishes to use a bugfix release. I believe this script is intended for SDKs 9.2 and newer. This means it is not the right choice for 10.0 SDK or corresponding artifacts

      I think your installed SDK is fine. Please update TIDL_TOOLS by upgrading the edgeai-benchmark repo to r10.0 or by replacing the tools using the link above, untarred into edgeai-benchmark/tools/AM62A

      • this edgeai-benchmark version is part of the edgeai-tensorlab/ repo. The standalone edgeai-benchmark repo only tracks up to 9.2 SDK. It is preferred to update your tools using the setup script in the 10.0 version-tagged repo 

      BR,
      Reese

    • Got it, succeed to run in npu ,but get wrong results.So i tried to run onnx model in cpu ,the get this.

      Details:

      download  yolov5s6_640_ti_lite_37p4_56p0.pt  from modelzoo

      ①edgeai-yolov5:

       python export.py --weights yolov5s6_640_ti_lite_37p4_56p0.pt  --img 640 --batch 1 --simplify --export-nms --opset 11
      get onnx and prototxt

      ②edgeai-benchmark(10.0):
      ./run_custom_pu.sh AM62A
      remain this in edgeai-benchmark/scripts/benchmark_custom.py
      'imagedet-7': dict(
      task_type='detection',
      calibration_dataset=imagedet_calib_dataset,
      input_dataset=imagedet_val_dataset,
      preprocess=preproc_transforms.get_transform_onnx(640, 640, resize_with_pad=True, backend='cv2', pad_color=[114,114,114]),
      session=sessions.ONNXRTSession(**utils.dict_update(onnx_session_cfg, input_optimization=False, input_mean=(0.0, 0.0, 0.0), input_scale=(0.003921568627, 0.003921568627, 0.003921568627)),
      runtime_options=settings.runtime_options_onnx_np2(
      det_options=True, ext_options={'object_detection:meta_arch_type': 6,
      'object_detection:meta_layers_names_list':f'/home/zxb/Desktop/ti/yolov5s6_640_ti_lite_37p4_56p0.prototxt',
      'advanced_options:output_feature_16bit_names_list':''
      }),
      model_path=f'/home/zxb/Desktop/ti/yolov5s6_640_ti_lite_37p4_56p0.onnx'),
      postprocess=postproc_transforms.get_transform_detection_yolov5_onnx(squeeze_axis=None, normalized_detections=False, resize_with_pad=True, formatter=postprocess.DetectionBoxSL2BoxLS()), #TODO: check this
      metric=dict(label_offset_pred=datasets.coco_det_label_offset_80to90(label_offset=1)),
      model_info=dict(metric_reference={'accuracy_ap[.5:.95]%':37.4})
      ),

      ③copy imagedet-7_onnxrt_Desktop_ti_yolov5s6_640_ti_lite_37p4_56p0_onnx.tar.gz to AM62A


      runtime_options = {
      "tidl_tools_path": "/home/tidl-tools",
      "artifacts_folder": "/home/yolov5s/artifacts",
      #"core_number": 1,
      }
      sess_options = onnxruntime.SessionOptions()
      sess_options.log_severity_level=3
      ep_list = ["TIDLExecutionProvider", 'CPUExecutionProvider']
      session = onnxruntime.InferenceSession(
      "/home/yolov5s/model/yolov5s6_640_ti_lite_37p4_56p0.onnx",
      providers=ep_list,
      provider_options=[runtime_options, {}],
      sess_options=sess_options,
      )
      # ['TIDLExecutionProvider', 'TIDLCompilationProvider', 'CPUExecutionProvider']
      #session = onnxruntime.InferenceSession(args.model,providers=['TIDLCompilationProvider'])
      start=time.time()
      ort_inputs = {session.get_inputs()[0].name: img[None, :, :, :]}
      output = session.run(None, ort_inputs)




      Is there anything wrong?
    • Hello, 

      Hmm, so you have downloaded TI's pretrained version of the model and exported to ONNX, and the results with CPU-only are wrong. If CPU results are wrong, then I expected compiled version on target will be as well.

      When you run on CPU (CPUExecutionProvider), are you preprocessing the image the same as it was during training? One of the main tasks is to subtract a mean (0 here, so nothing to do) and multiply by a scaler (I see 0.00392 for each channel). Cropping / resizing are less important. 

      preprocess=preproc_transforms.get_transform_onnx(640, 640, resize_with_pad=True, backend='cv2', pad_color=[114,114,114]),

      Did you pull the pretrained versions from links here? : https://github.com/TexasInstruments/edgeai-yolov5/tree/4d86a53a0a25ca8f9e6fa4882b1096ade2bc9839/pretrained_models/models/detection/coco/edgeai-yolov5-gplv3 

      BR,
      Reese

    • Sure,http://software-dl.ti.com/jacinto7/esd/modelzoo/gplv3/latest/edgeai-yolov5/pretrained_models/models/detection/coco/edgeai-yolov5/yolov5s6_640_ti_lite_37p4_56p0.pt    

      (mini) PS D:\zxb\accc\edgeai-yolov5-main> python export.py --weights yolov5s6_640_ti_lite_37p4_56p0.pt --img 640 --batch 1 --simplify --export-nms --opset 11
      export: weights=yolov5s6_640_ti_lite_37p4_56p0.pt, img_size=[640], batch_size=1, device=cpu, include=['torchscript', 'onnx', 'coreml'], half=False, inplace=False, train=False, optimize=False, dynamic=False, simplify=True, opset=11, export_nms=True
      YOLOv5 2024-8-5 torch 1.9.0+cpu CPU

      Fusing layers...
      C:\Users\Admin\.conda\envs\mini\lib\site-packages\torch\nn\functional.py:718: UserWarning: Named tensors and all their associated APIs are an experimental feature and subject to change. Please do not use them for anything important until they are released as stable. (Triggered internally at ..\c10/core/TensorImpl.h:1156.)
      return torch.max_pool2d(input, kernel_size, stride, padding, dilation, ceil_mode)
      Model Summary: 297 layers, 12653932 parameters, 0 gradients, 17.4 GFLOPs

      PyTorch: starting from yolov5s6_640_ti_lite_37p4_56p0.pt (25.7 MB)

      TorchScript: starting export with torch 1.9.0+cpu...
      D:\zxb\accc\edgeai-yolov5-main\models\yolo.py:57: TracerWarning: Converting a tensor to a Python boolean might cause the trace to be incorrect. We can't record the data flow of Python values, so this value will be treated as a constant in the future. This means that the trace might not generalize to other inputs!
      if self.grid[i].shape[2:4] != x[i].shape[2:4] or self.onnx_dynamic:
      TorchScript: export success, saved as yolov5s6_640_ti_lite_37p4_56p0.torchscript.pt (51.1 MB)

      ONNX: starting export with onnx 1.17.0...
      D:\zxb\accc\edgeai-yolov5-main\utils\general.py:593: TracerWarning: Iterating over a tensor might cause the trace to be incorrect. Passing a tensor of different shape won't change the number of iterations executed (and might lead to errors or silently give incorrect results).
      for xi, x in enumerate(prediction): # image index, image inference
      C:\Users\Admin\.conda\envs\mini\lib\site-packages\torch\onnx\symbolic_opset9.py:697: UserWarning: This model contains a squeeze operation on dimension 1 on an input with unknown shape. Note that if
      the size of dimension 1 of the input is not 1, the ONNX model will return an error. Opset version 11 supports squeezing on non-singleton dimensions, it is recommended to export this model using opset version 11 or higher.
      warnings.warn("This model contains a squeeze operation on dimension " + str(squeeze_dim) + " on an input " +
      ONNX: simplifying with onnx-simplifier 0.4.36...
      ONNX: export success, saved as yolov5s6_640_ti_lite_37p4_56p0.onnx (50.7 MB)
      ONNX: run --dynamic ONNX model inference with detect.py: 'python detect.py --weights yolov5s6_640_ti_lite_37p4_56p0.onnx'
      Minimum required torch version for importing coremltools.optimize.torch is 2.1.0. Got torch version 1.9.0.
      Fail to import BlobReader from libmilstoragepython. No module named 'coremltools.libmilstoragepython'

      CoreML: export failure: module 'torch' has no attribute 'fx'

      Export complete (7.21s). Visualize with github.com/.../netron.

    • V8:

       

      (mmyolo) PS D:\zxb\accc\test\mmyolo> python projects/easydeploy/tools/export_onnx.py  .\configs\yolov8\yolov8_n_syncbn_fast_8xb16-500e_coco.py  .\mmyolov8n.pth  --work-dir .\tests\  --img-size 640 640 --simplify   --iou-threshold 0.65  --score-threshold 0.25 --opset 11 --backend ONNXRUNTIME --export-type MMYOLO

      Export ONNX with bbox decoder and NMS ...                                                                         11 --backend ONNXRUNTIME --export-type MMYOLO;cabd5a98-aa67-45ba-bed2-33e35e38e5a6

      Loads checkpoint by local backend from path: .\mmyolov8n.pth

      C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\mmdet\apis\inference.py:90: UserWarning: dataset_meta or class names are not saved in the checkpoint's meta data, use COCO classes by default.

      C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\edgeai_torchmodelopt\xmodelopt\surgery\v1\convert_to_lite.py:166: UserWarning: WARNING - xnn.surgery is based on the modules. For superior functionality, please use the torch.fx based xmodelopt.surgery instead

        warnings.warn("WARNING - xnn.surgery is based on the modules. For superior functionality, please use the torch.fx based xmodelopt.surgery instead")

      Loads checkpoint by local backend from path: .\mmyolov8n.pth

      C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\torch\functional.py:504: UserWarning: torch.meshgrid: in an upcoming release, it will be required to pass the indexing argument. (Triggered internally at ..\aten\src\ATen\native\TensorShape.cpp:3484.)

        return _VF.meshgrid(tensors, **kwargs)  # type: ignore[attr-defined]

      d:\zxb\accc\test\mmyolo\mmyolo\models\task_modules\coders\distance_point_bbox_coder.py:45: TracerWarning: Converting a tensor to a Python boolean might cause the trace to be incorrect. We can't record the data flow of Python values, so this value will be treated as a constant in the future. This means that the trace might not generalize to other inputs!

        assert points.size(-2) == pred_bboxes.size(-2)

      d:\zxb\accc\test\mmyolo\projects\easydeploy\nms\ort_nms.py:114: TracerWarning: torch.tensor results are registered as constants in the trace. You can safely ignore this warning if you use this function to create tensors out of constant variables that would be the same every time you call this function. In any other case, this might cause the trace to be incorrect.

        max_output_boxes_per_class = torch.tensor([max_output_boxes_per_class])

      C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\torch\onnx\symbolic_opset9.py:5589: UserWarning: Exporting aten::index operator of advanced indexing in opset 11 is achieved by combination of multiple ONNX operators, including Reshape, Transpose, Concat, and Gather. If indices include negative values, the exported graph will produce incorrect results.

        warnings.warn(

      ============= Diagnostic Run torch.onnx.export version 2.0.1+cu118 =============

      verbose: False, log level: Level.ERROR

      ======================= 0 NONE 0 NOTE 0 WARNING 0 ERROR ========================

       

      ONNX export success, save into .\tests\mmyolov8n.onnx

      Converted model is invalid: Nodes in a graph must be topologically sorted, however input '275' of node:

      name: 276 OpType: Greater

       is not output of any previous nodes.

      Prototxt export success, save into .\tests\mmyolov8n.prototxt

       

       

       

      Patch  mmyolo with  0001-2024-Aug-2-mmyolo.commit-8c4d9dc5.-model-surgery-with-edgeai-modeloptimization.txt

      Cnt detect anything

       

      [After patch]

       

      [Before patch]

       

      then i find that output nodes after surgeon can't be searched,only scores node,this seems to the problem of mmyolo.

      How can i  get the same model like  modelzoo yolov8n.

    • Hello,

      I am asking a few other members of our team to take a look here, since this is deeper into these tools than I am equipped to help with. I have not been able to reproduce your errors on my machine (ubuntu 22.04).

      I'd like to take a moment to summarize where we are:

      • Attempted model training for several YOLO archicetures
        • yolov8 using mmyolo + TI patches. Status: Model may be exported, but is not making correct detections
        • yolov5 using edgeai-yolov5 repo from TI. Status: ONNX model exported but failing for prototxt -- looks like dependency error
        • yolox with modelmaker (archived version of repo, not part of tensorlab). Status: Model trained on tidrivingscapes dataset, fails during compilation
      • encounter variety of dependency errors.

      I should have noticed this sooner, but looks like your paths are Windows. Are you running on a Windows OS? These tools are validated against Ubuntu. Release versions <9.0 would be validated for Ubutnu 18.04 and >=9.0 on Ubuntu 22.04. 

      BR,
      Reese

    • Hello

      The problem with the modelmaker-cpu has been solved. So it's still there now

      • yolov8 uses mmyolo + TI patches. Status: The model may have been exported, but it was not detected correctly. Since the exported ONNX model cannot be detected correctly, the artifact must also be wrong.
      • yolov5 uses TI's edgeai-yolov5 repository. Status: The onnx model has been exported, but prototxt fails -- it looks like a dependency error.
      • modelmaker of yolox when i  use gpu to train ,it ends in export onnx model. It can be trained  ,but cant exportonnx.Here is the log.
      • (cd modelmaker and vi setup_all.sh  and replace setup_cpu.sh -> setup.sh)modelmakrlog.txt

      Question1 about v8 i have tried in ubuntu 22.04 it comes with the problems, wrong detection,cant be searched output nodes

      Since our model include  face detection with 5 keypoints, im tring to  find a way to convert  v5/v8 pt -> pth  -> onnx  -> artifacts.But abolve all failed.I will try later  v5 in ubuntu22.04 today.Thanks for following up on this issue

    • Hello,

      Since  the dms project is going to be produced in April, the overall situation is in a hurry, and I may have more questions  in the process of development.Sorry to trouble you again.

      Two more questions ,these code i copied from e2e 'ti engineer can't run.  Is there anyother gst examples? Or simple ways to rebuild opencv imshow in AM62A. 

      import cv2
      import numpy as np

      width = 640
      height = 480
      GST_PIPE = f'appsrc caps="video/x-raw,width={width},height={height},format=RGB,framerate=30/1" ! kmssink driver-name=tidss sync=false'
      video_out = cv2.VideoWriter(GST_PIPE, cv2.CAP_GSTREAMER, 0, 30, (width, height), True)

      while True:
          frame = np.random.randint(255, size=(height, width, 3), dtype=np.uint8)
          video_out.write(frame)
      video_out.release()
      Question 2:
           How can i remove logo of   edgeai-gst-apps  from top left corner ,i checked all the cpp code can't find.
    • I was looking at your error log from modelmaker:

      RuntimeError: Input type (torch.cuda.ByteTensor) and weight type (torch.FloatTensor) should be the same

      From your explanation, I understood that it works fine in CPU mode, but you tried in GPU mode and it did not work. We have been recommending the default installation mode i.e. CPU and have not recently tested the GPU mode - it's possible that there could be and issue in GPU mode. I guess you are not waiting for a solution to this, since you have the default CPU model already working.

      How about the compilation of yolox model from modelmaker - modelmaker produces the compiled output - is it working?

    • Hello

      The problem with the modelmaker-cpu has been solved. So it's still there now

      • (cd modelmaker and vi setup_all.sh  and replace setup_cpu.sh -> setup.sh)modelmakrlog.txt

      Please confirm:

      • Model export when training with GPU fails.
      • Model training and export with CPU passes

      and you mention yolov8 completes training, but detection results are poor. Perhaps  More epochs / training data is needed to handle the modified layers. Can you pass the logs for the training + model export of yolov8?

      I've asked another expert to help with the training/export task. I can help with other portions like evaluating the model on live input.

      Model testing/eval on target:

      opencv.imshow will be quite slow due to lack of GPU on this processor. The "weston/wayland" window compositor is slow on Am62A due to CPU rendering, and gstreamer --> KMS-sink is generally preferred.

      edgeai-gst-apps repo is a good example overall.. The gstreamer pipeline is created from a YAML config file, and then TIDL/ deep learning + postprocessing is handled from the infer_pipe.py script

      I have produced a few other demos that show how gstreamer string can be built and run. This script is less complex than the edgeai-gst-apps since it is building a specific pipeline rather than basing the structure on a YAML file -- see here for another GST example:

      video_out = cv2.VideoWriter(GST_PIPE, cv2.CAP_GSTREAMER, 0, 30, (width, height), True)

      while True:
          frame = np.random.randint(255, size=(height, width, 3), dtype=np.uint8)
          video_out.write(frame)

      Does this work approach for you?

           How can i remove logo of   edgeai-gst-apps  from top left corner ,i checked all the cpp code can't find.

      In the YAML config file you pass, set the 'title' to be an empty string. This will remove one part of the name / logo. 

      For the other part (Texas Instruments Edge AI), you will need to add one small change to the code. In apps_python/gst_wrapper,  set the 'main-title' property to an empty string (' ') for the tiperfoverlay element, like so: 

      Fullscreen
      1
      2
      3
      4
      5
      6
      if output.overlay_perf_type != None:
      sink_elements += make_element("queue")
      property = {"title":output.title,
      "main-title": " ",
      "overlay-type":output.overlay_perf_type}
      sink_elements += make_element("tiperfoverlay",property=property)
      XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

      BR,
      Reese

    • output  of CPU can work

    • Thanks,

      This also works in apps_cpp.  modelmaker    :     it seems  config_keypoint_detection.yaml  dosent work      

      Please check if the given model_name is valid :yolox_s_keypoint.

    • Regarding Keypoint detection - Keypoint detection implementation is being updated - it is expected to work in the upcoming 10.1 release, expected Mid January.

    • Hi,

       Going back to my original question, if I only have an onnx model and weights pt file, how do I go about getting it to run on the NPU.

      We want some instructions.

      Since edgeaitensorlab only provided yolov5 and mmyolo mmdetection and so on.In the preview problems ,i used mmyolo to get onnx and prototxt,onnx can't  detect and  can't be compiled,here are the models which we gived to FAE who told us to wait for ti-engineer provide instructions 2weeks ago.

      mmyolov8n.zip

       

      V8:

       

      (mmyolo) PS D:\zxb\accc\test\mmyolo> python projects/easydeploy/tools/export_onnx.py  .\configs\yolov8\yolov8_n_syncbn_fast_8xb16-500e_coco.py  .\mmyolov8n.pth  --work-dir .\tests\  --img-size 640 640 --simplify   --iou-threshold 0.65  --score-threshold 0.25 --opset 11 --backend ONNXRUNTIME --export-type MMYOLO

      Export ONNX with bbox decoder and NMS ...                                                                         11 --backend ONNXRUNTIME --export-type MMYOLO;cabd5a98-aa67-45ba-bed2-33e35e38e5a6

      Loads checkpoint by local backend from path: .\mmyolov8n.pth

      C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\mmdet\apis\inference.py:90: UserWarning: dataset_meta or class names are not saved in the checkpoint's meta data, use COCO classes by default.

      C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\edgeai_torchmodelopt\xmodelopt\surgery\v1\convert_to_lite.py:166: UserWarning: WARNING - xnn.surgery is based on the modules. For superior functionality, please use the torch.fx based xmodelopt.surgery instead

        warnings.warn("WARNING - xnn.surgery is based on the modules. For superior functionality, please use the torch.fx based xmodelopt.surgery instead")

      Loads checkpoint by local backend from path: .\mmyolov8n.pth

      C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\torch\functional.py:504: UserWarning: torch.meshgrid: in an upcoming release, it will be required to pass the indexing argument. (Triggered internally at ..\aten\src\ATen\native\TensorShape.cpp:3484.)

        return _VF.meshgrid(tensors, **kwargs)  # type: ignore[attr-defined]

      d:\zxb\accc\test\mmyolo\mmyolo\models\task_modules\coders\distance_point_bbox_coder.py:45: TracerWarning: Converting a tensor to a Python boolean might cause the trace to be incorrect. We can't record the data flow of Python values, so this value will be treated as a constant in the future. This means that the trace might not generalize to other inputs!

        assert points.size(-2) == pred_bboxes.size(-2)

      d:\zxb\accc\test\mmyolo\projects\easydeploy\nms\ort_nms.py:114: TracerWarning: torch.tensor results are registered as constants in the trace. You can safely ignore this warning if you use this function to create tensors out of constant variables that would be the same every time you call this function. In any other case, this might cause the trace to be incorrect.

        max_output_boxes_per_class = torch.tensor([max_output_boxes_per_class])

      C:\Users\Admin\.conda\envs\mmyolo\lib\site-packages\torch\onnx\symbolic_opset9.py:5589: UserWarning: Exporting aten::index operator of advanced indexing in opset 11 is achieved by combination of multiple ONNX operators, including Reshape, Transpose, Concat, and Gather. If indices include negative values, the exported graph will produce incorrect results.

        warnings.warn(

      ============= Diagnostic Run torch.onnx.export version 2.0.1+cu118 =============

      verbose: False, log level: Level.ERROR

      ======================= 0 NONE 0 NOTE 0 WARNING 0 ERROR ========================

       

      ONNX export success, save into .\tests\mmyolov8n.onnx

      Converted model is invalid: Nodes in a graph must be topologically sorted, however input '275' of node:

      name: 276 OpType: Greater

       is not output of any previous nodes.

      Prototxt export success, save into .\tests\mmyolov8n.prototxt

       

       

       

      Patch  mmyolo with  0001-2024-Aug-2-mmyolo.commit-8c4d9dc5.-model-surgery-with-edgeai-modeloptimization.txt

      Cnt detect anything

       

      [After patch]

       

      [Before patch]

       

      then i find that output nodes after surgeon can't be searched,only scores node,this seems to the problem of mmyolo.

      How can i  get the same model like  modelzoo yolov8n.

      Also i used edgeai-yolov5    python=3.9   install requirements and follow readme.md  using "python export.py --weights .\pretrained_models\yolov5s_640_ti_lite\weights\yolov5s6_640_ti_lite_37p4_56p0.pt   --img 640 --batch 1 --simplify --export-nms --opset 11"

      It can't works too.

       

    • Merry Christmas,

      Our DMS project base on edgeai-gst-apps are almost finished,with 2flows running on cpu and 1flows running on npu,the last custom model also need  to be run on npu so that can satisfy the auto requirements,but we have encountered some other problems based on the above issues.We indeed need someone who can look deep into these questions.

    • This is one of the DMS models using edgeai-tidl-tools , calibration 11 pictures 5epoch,remains  some error between the two sets of data.

      How can i change the calibration epoch to 20 or more.

    • Hi 

      I wonder what is the status for this problem now. Have you got through the pipeline of pth -> onnx -> aritifacts? 

      This seems to be saying there is accuracy loss in onnx->artifacts. So the major problem now becomes accuracy loss in quantization process. Am I correct? 

      ,remains  some error between the two sets of dat

      Regards,

      Adam

    • Hi 

      This isn't a od/kpt type model.I referenced other replies on  e2e to get these artifacts using edgeai-tidl-tools:  task_type: classfication  without prototxt. 

      Questions above about od type  have not been resolved.During this 2weeks, there were other problems similar to the ones above.Like:onnxruntime.capi.onnxruntime_pybind11_state.InvalidArgument: [ONNXRuntimeError] : 2 : INVALID_ARGUMENT : Non-zero status code returned while running MaxPool node. Name:'/baseModel/backbone/stage4/stage4.2/poolings/MaxPool' Status Message: Unsupported pooling size.

      This artifacts file was obtained via edgeai-benchmark.But it can pass fixed-point Calibration and infer.

    • Hello Wang Xiaojun,

      I see your challenges with YOLO-based models here. I similarly see export issue on my machine using Python 3.8 with Ubuntu 22.04 LTS. 

      YOLOv5

      I have dependency challenges with yolov5 using the default settings / installation scripts.

      The Coremltools package seems to give the most trouble -- I notice the requirements set the version to >=4.1, and my machine installed a version >8.0. I reinstalled specifically to 6.1 -- we need to restrict the maximum version for this. Please find here my full list of installed packages for python 3.8: 

      With these versions installed, I'm able to complete the export and acquire ONNX and PROTOTXT files. I am then able to compile/import with edgeai-tidl-tools, and verify that some relevant objects were detected (resulting image below, although I note slight difference from CPU-based inference)

      Note that I am using TI's provided .PT file as the starting point of the export command (same as you noted, and present in the README.md of edgeai-yolov5). 

      YOLOv8 w/ patched mmyolo

       

      Patch  mmyolo with  0001-2024-Aug-2-mmyolo.commit-8c4d9dc5.-model-surgery-with-edgeai-modeloptimization.txt

      Cnt detect anything

      So you have applied this patch and exported the model, and it does not make correct detections. After you applied the patch, did you train the model for any further epochs (yes or no)? The model optimizations replace several layers such that further training is required. If you did not retrain, this may explain lack of detection

      I have not yet validated this one myself.

      Other DMS models

      This is one of the DMS models using edgeai-tidl-tools , calibration 11 pictures 5epoch,remains  some error between the two sets of data.

      How can i change the calibration epoch to 20 or more.

      I believe you want the quantization step to run more calibration iterations. There is an option for the calibration frames (how many images to pass) and how many calibration iterations (for each frame, N iterations). You should set the option for the latter, 'advanced_options:calibration_iterations' to a higher value. Doc here:

      Questions above about od type  have not been resolved.During this 2weeks, there were other problems similar to the ones above.Like:onnxruntime.capi.onnxruntime_pybind11_state.InvalidArgument: [ONNXRuntimeError] : 2 : INVALID_ARGUMENT : Non-zero status code returned while running MaxPool node. Name:'/baseModel/backbone/stage4/stage4.2/poolings/MaxPool' Status Message: Unsupported pooling size.

      What is the kernel size and other attributes for this layer? Up to 3x3 is supported, and larger (odd) kernels are emulated by creating multiple MaxPools in sequential order. Several small kernels in order can perform the same operation as one larger kernel. The image is too blurry for me to see the tensor sizes.

      This thread is quite long and hard to track. If there is a clear way to break this into separate topics as new threads, that would help our support team.