This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FPGA Configuration & AM3505 Reference Design

Other Parts Discussed in Thread: AM3505

Dear All,

I am planning to use the AM3505 processor to configure a Cyclone IV FPGA. The FPGA configuration scheme is PS. The FPGA's firmware is stored on a NAND flash or SD card connencted to the AM3505. The file format is a raw binary file (.rbf).

I thought that I can use some of the GPIO's to configure the FPGA. I need a clock output (f<100MHz), data output and some control and status bits.

Do you think this is feasible?

Is there any application note for FPGA configuration using AM3505?

Do you know where to find a reference design, preferable schematic, using the AM3505.

Thanks!