Hi,
I need the Allegro .brd-file for the new ICE V2.1a version to build a add-on board. If i use the link to the PCB-files I can find the schematics and the BOM but not the board-file.
The files for the older ICE V1.0 version I used bevor were in sprr171.
Regards,
Klaus
ps: This is the like I used for the PCB-files:http://processors.wiki.ti.com/index.php/AM335x_Industrial_Communications_Engine_Board_Design_Files#Rev_2.1A