Tool/software: Code Composer Studio
Hello,
does the DSK5509A run with CCS v7 on a 64-bit-system (windows 10).
Are there any example codes working with that setup?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
does the DSK5509A run with CCS v7 on a 64-bit-system (windows 10).
Are there any example codes working with that setup?
Thank you
Elisabeth,
As Mukul had iterated previously, its highly recommended to use a newer C55x device if possible.
Apologies for the trouble you are having with this. Let me try to provide more info that I was able to dig up.
There is an older TI c55x CSL located here for the C5509 http://www.ti.com/tool/sprc133. Please download C55XCSL-SPRC133.
I was able to build the examples in this package in CCSv6 with Windows 7. I can't say for sure what the outcome will be with Win 10, but I don't think this would be a problem.
The example I built from the above mentioned package is C:\Program Files\C55xxCSL\examples\generic5509\csl\timer\timer1\timer1
You will need to use the "Import Legacy CCS v3.3 CCS projects" under Project in CCS. Navigate to the .pjt project that you want to import and pull it into your workspace. Something you want to keep in mind is that in order to build the examples without errors, you will have to follow the document under C:\Program Files\C55xxCSL\doc\Releasenote.htm. This gives instructions on what project properties you will need to manipulate in order to build, especially section 3. Setting up build environment to use CSL.
Lali