Error 0x80000260/-1137
Fatal Error during: Execution, Initialization, OCS,
It appears that the target is being held in reset. This may be
due to Wait-In-Reset (WIR) configuration set by the EMU0=0
and EMU1=1 pin settings. If this is the case, DISCONNECT
all CONNECTED devices including icepick and then select
RETRY to clear the WIR configuration.
If this is a multi-core system, the master CPU may not be
releasing the DSP/MCU from reset. Please check your
configuration in CC_setup and/or your GEL file to ensure that
nothing is blocking the DSP/MCU from being released from reset
I/O Port = 510
Board Name: DAVINCI_HD_1080p_XDS510USB
Cpu Name: C64PLUS
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
----------------------------------------------------------------------------------
-----------------------------------------------------------------------------
1, software configuration:
my CCS version is 3.3.81.6.
I already installed setupCCSPlatinum_v30330.ZIP and Patch_030330_XDS510USB_22sept2010.zip (downloaded from http://support.spectrumdigital.com/ccs33/)
Davinci™ HD1080p EVM CCS Config Files, Davinci™ HD1080p EVM DSP GEL File and Davinci™ HD1080p EVM CCS Config Files
downloaded from http://support.spectrumdigital.com/boards/evmdm6467t/revc/.
2, my hardware configruation are below:
JTAG Emulators is spectrum digital XDS510 USB Plus.
Switch SW3 configuration is ALL(8 pin) is off.
S1,EMU0/1 Select Swtich configuration is EMU0 (H) and EMU1(H).
Dear Experts:
will you please tell me what 's the problem ? thanks.