Part Number: PROCESSOR-SDK-DRA7X
Tool/software: TI C/C++ Compiler
Hi Brijesh,
Previous Ticket :
https://e2e.ti.com/support/processors/f/791/t/860813#pi320966=2
We have already tested with BSP API"s its not changing.
Bsp_PlatformVencSrc vencClkCfg;
vencClkCfg.vencClkSrc = BSP_PLATFORM_CLKSRC_DPLL_HDMI;
vencClkCfg.outputVenc = BSP_PLATFORM_VENC_LCD2 /* We are using LCD 2 */
Bsp_platformSetVencClkSrc(&vencClkCfg);
Below is the usecase.
Path: /home/workspace/3dot4/vision_sdk/apps/src/rtos/usecases/weston_dualcamera_dsswb
UseCase: weston_dualcamera_dsswb
Capture -> Display_Video
Capture_1 -> Display_Video1
DispDistSrc_gfx -> Display_gfx
DispDistSrc_vid3 -> Display_vid3
Capture_dsswb -> Alg_SwCrc
Testing:
After making the changes, could'nt see any difference. Verification is done by checking below register values.
DSS_CTRL: 0x5800 0040
root@mmt2020-a880:~# omapconf read 0x58000040
00011000
Bit 12: LCD2_CLK_SWITCH is 1 (0x1: DPLL_DSI1_B_CLK1 selected)
/* MUX CONTROL for PLL */
CTRL_CORE_DSS_PLL_CONTROL
root@mmt2020-a880:~# omapconf read 0x4A002538
00000288
Bit: 6:5: DSI1_B_CLK1_SELECTION is 0 (0x0 = DPLL_VIDEO1).
Regards,
Raghu