Part Number: AM6548
Does AM65 support Ethernet Switch on Linux or RTOS platform ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM6548
Does AM65 support Ethernet Switch on Linux or RTOS platform ?
Currently AM65x does not support Ethernet Switch on either Linux or RTOS but there is support provided for Dual MAC out of the box.
For Linux support, see this documentation
For RTOS support, please check the ICSS EMAC loopback application inside pdk/packages/ti/drv/emac/test. It can be built through the following steps
1. go to pdk/packages --> source pdksetupenv.sh
2. go to pdk/packages/ti/drv/emac --> make
3. Binary will be in packages/ti/binary/Emac_Icssg_TestApp
RGMII/MII support
NOTE : There are plans to add support for 100Mbps Ethernet/IP on ICSSG on RTOS by Nov End 2021. Ethernet/IP can be used as a switch proxy since it supports most switch functionalities. For details, refer to the User Guide and Datasheet
Regards
Vineet