This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM5749: am5749/am57x eMMC cannot boot with fat mode.

Part Number: AM5749


Hi, All:

I got some hole/trap with am5749_IDK eMMC boot with fat mode.
I saw some unsolved thread on forum.
Thus, I write down the note for someone get the same hole/trap.
I will close the thread tomorrow.

//---root cause
am5749 supports eMMC boot with 2 mode:
1.fat mode
2.raw mode

The eMMC fat mode, the partition must be:
Type: W95 FAT32
ID: c
and this partition should be set bootable flag.

The hole/trap is :
Usually, the fdisk creates partition with ID:83/type:Linux.
It is must to change partition from ID:83/type:Linux to ID:c/type:W95 FAT32

Below is operation note for fat mode and raw mode:



//---environment
[Board] am5749 IDK
[SDK] ti-processor-sdk-linux-am57xx-evm-06.03.00.106-Linux-x86-Install.bin
[Hardware rework]
The am5749_IDK, the sysboot default is 0x8106.
Booting devices order is
1:SD
2:QSPI_1

Changin sysboot from 0x8106 to 0x8102.
(Moving resistor from R436 to R455)
Booting devices order is
1:USB
2:SD
3:eMMC


//---operation note
[fat mode]

Plug in SD card and boot to linux.
SD card is /dev/mmcblk0
eMMC is /dev/mmcblk1

clear eMMC 1M bytes
    dd if=/dev/zero of=/dev/mmcblk1 bs=512 count=2K
    sync
    reboot

check status of eMMC
    fdisk -l /dev/mmcblk1
Disk /dev/mmcblk1: 14.8 GiB, 15913189376 bytes, 31080448 sectors                                                       
Units: sectors of 1 * 512 = 512 bytes                                                                                  
Sector size (logical/physical): 512 bytes / 512 bytes                                                                  
I/O size (minimum/optimal): 512 bytes / 512 bytes

create partition on eMMC
    fdisk /dev/mmcblk1

list status of eMMC
    p
Disk /dev/mmcblk1: 14.8 GiB, 15913189376 bytes, 31080448 sectors                                                       
Units: sectors of 1 * 512 = 512 bytes                                                                                  
Sector size (logical/physical): 512 bytes / 512 bytes                                                                  
I/O size (minimum/optimal): 512 bytes / 512 bytes                                                                      
Disklabel type: dos                                                                                                    
Disk identifier: 0x5b9b8212

create a new empty DOS partition table
    o                                                                                                
Created a new DOS disklabel with disk identifier 0x76a6abe2.

create partition#1
    n
    p
    1
    2048
    +70M

list status of eMMC
    p
Device         Boot Start    End Sectors Size Id Type                                                                  
/dev/mmcblk1p1       2048 145407  143360  70M 83 Linux


change partition#1 type from linux to dos
t
c

list status of eMMC
    p
Device         Boot Start    End Sectors Size Id Type                                                                  
/dev/mmcblk1p1       2048 145407  143360  70M  c W95 FAT32 (LBA)

set bootable flag
    a

list status of eMMC
    p
Device         Boot Start    End Sectors Size Id Type                                                                  
/dev/mmcblk1p1 *     2048 145407  143360  70M  c W95 FAT32 (LBA)

create partition#2
    n
    p
    2
    [enter]
    [enter]

list status of eMMC
    p   
Device         Boot  Start      End  Sectors  Size Id Type                                                             
/dev/mmcblk1p1 *      2048   145407   143360   70M  c W95 FAT32 (LBA)                                                  
/dev/mmcblk1p2      145408 31080447 30935040 14.8G 83 Linux  

write to /dev/mmcblk1
    w

format filesystem
    mkfs.fat /dev/mmcblk1p1 -n boot
    mkfs.ext4 /dev/mmcblk1p2 -L rootfs

reboot and auto mount mmcblk1p1 & mmcblk1p2 to /run/media
    reboot

copy boot and rootfs to mmcblk1p1 & mmcblk1p2.
There is a trick method:
 create a am5749_IDK SD card with SDK.
 Plug in the SD card in USB with card reader.
 My case, the device node is located at /run/media/sda1 and /run/media/sda2.
    cp /run/media/sda1/* /run/media/mmcblk1p1
    cp /run/media/sda2/* /run/media/mmcblk1p2 -r
    sync

Press and hold reset button.
Remove SD card
Release reset button and test eMMC boot with fat mode.


[raw mode]

Plug in SD card and boot to linux.
SD card is /dev/mmcblk0
eMMC is /dev/mmcblk1

clear eMMC 1M bytes
    dd if=/dev/zero of=/dev/mmcblk1 bs=512 count=2K
    sync
    reboot

dump MLO to eMMC at 0x100 sector, ROM will get it.
    dd if=/run/media/mmcblk0p1/MLO of=/dev/mmcblk1 bs=512 seek=256

dump uboot.img to eMMC at 0x300 sector, MLO will get it.
    dd if=/run/media/mmcblk0p1/u-boot.img of=/dev/mmcblk1 bs=512 seek=768

create file system on eMMC.
In order to keep zone for uboot.ing, first partition must start at 4096 instead of 2048.
create partition on eMMC
    fdisk /dev/mmcblk1

list status of eMMC
    p
Disk /dev/mmcblk1: 14.8 GiB, 15913189376 bytes, 31080448 sectors                                                       
Units: sectors of 1 * 512 = 512 bytes                                                                                  
Sector size (logical/physical): 512 bytes / 512 bytes                                                                  
I/O size (minimum/optimal): 512 bytes / 512 bytes                                                                      
Disklabel type: dos                                                                                                    
Disk identifier: 0x8d681464


create a new empty DOS partition table
    o                                                                                                
Created a new DOS disklabel with disk identifier 0x875af9a3.

create partition#1
    n
    p
    1
    4096
    +70M

list status of eMMC
    p
Device         Boot Start    End Sectors Size Id Type                                                                  
/dev/mmcblk1p1       4096 147455  143360  70M 83 Linux

change partition#1 type from linux to dos
t
c

list status of eMMC
    p
Device         Boot Start    End Sectors Size Id Type                                                                  
/dev/mmcblk1p1       4096 147455  143360  70M  c W95 FAT32 (LBA)

set bootable flag
    a

list status of eMMC
    p
Device         Boot Start    End Sectors Size Id Type                                                                  
/dev/mmcblk1p1 *     4096 147455  143360  70M  c W95 FAT32 (LBA)

create partition#2,
!!! Caution !!! the First setor is NOT 2048.
First setor is next to end of partition#1.
This case is 143360+1 = 143361
key in and fdisk will tell you
Sector 143361 is already allocated.                                                                                    
First sector (147456-31080447, default 147456)
    n
    p
    2
    147456
    [enter]

list status of eMMC
    p                                                                                                
Device         Boot  Start      End  Sectors  Size Id Type                                                             
/dev/mmcblk1p1 *      4096   147455   143360   70M  c W95 FAT32 (LBA)                                                  
/dev/mmcblk1p2      147456 31080447 30932992 14.8G 83 Linux

write to /dev/mmcblk1
    w

format filesystem
    mkfs.fat /dev/mmcblk1p1 -n boot
    mkfs.ext4 /dev/mmcblk1p2 -L rootfs

reboot and auto mount file system
partition #1 is vfat, empty it. just for compatibility.
partition #2 is ext4 for rootfs.
After running fdisk, mkfs.vfat, mkfs.ext4, and
reboot,
there are :
/run/media/mmcblk1p1
/run/media/mmcblk1p2
    reboot

copy rootfs to mmcblk1p2.
There is a trick method:
  create a am5749_IDK SD card with SDK.
  Plug in the SD card in USB with card reader.
  My case, the software location in /run/media/sda1 and /run/media/sda2.
copy all of file in /run/media/sda2 to mmcblk1p2.ext4
    cp  /run/media/sda2/* /run/media/mmcblk1p2 -r

Press and hold reset button.
Remove SD card
Release reset button and test eMMC boot with raw mode.


Wish everyone leave the office on time.

  • Hi Greatcat Chen,

    Thanks a bunch for writing the details and helping us with eMMC boot. I will try the steps and reply back here.

    Thanks,
    Keerthy

  • Hi, Keerthy:

    By the way, the SATA boot seems it is similer to eMMC boot.
    The am57x ROM supports SATA boot with raw mode and fat/HLO mode.
    But SDK 06.03.00.106 seems it does not support fully.
    The HLO can not load uboot with the below message.

    U-Boot SPL 2019.01-g333c3e72d3 (Apr 20 2020 - 04:15:00 +0000)                   
    DRA762-GP ES1.0 ABZ package                                                     
    no pinctrl state for default mode                                               
    Card did not respond to voltage select!                                         
    Firmware loading failed                                                         
    SPL: Unsupported Boot Device!                                                   
    SPL: failed to boot from all boot devices                                       
    ### ERROR ### Please RESET the board ###

    I'll open another thread for this. :)

    Best regards,
    Greatcat