Dear all
I have a question about RSSI range in AFE7988.
If RSSI range is 0 dB <= SNR, Pfs_cw, min =-0.4dBm (f=3.6G,DSA=0dB) and SFDR=84dBFS,
so is it OK to use RSSI = -0.4dBm to -84.4dBm (84dB) ?
On the ohter hand, there is an item of Psa_cw,max = 18.5dBm, (I don't understand this item.)
Is DSA=18.9dB(=19dB) setting in this case ?
And RSSI range becomes from 18.5dBm to -65.5dBm (84dB)?
vest regard