Other Parts Discussed in Thread: AWR2243, DCA1000EVM, UNIFLASH, AWR1243
Tool/software:
Hi All,
I'm working with the AWR2243BOOST, and I'm trying to connect via SPI using the mmWave Studio. However, I'm encountering an issue where the SPI connectivity status remains disconnected. Here's what I've done so far:
Firmware Loaded:
- Radar SS:
C:\ti\mmwave_studio_03_00_00_14\rf_eval_firmware\AWR2243_ES1_1\radarss\xwr22xx_radarss.bin
- Master SS:
C:\ti\mmwave_studio_03_00_00_14\rf_eval_firmware\AWR2243_ES1_1\masterss\xwr22xx_masterss.bin
Observed Issue: After attempting to connect via SPI, I receive an error, and the connectivity status shows as disconnected.
I am using the mmWave Studio version 03.00.00.14 and integrating the DCA1000EVM with the AWR2243BOOST board.
I am supplying power from the AWR2243BOOST (5V), and through the HD pin connector, the 5V is also supplied to the DCA1000EVM.
I am attaching the pics of Integrating the both boards
When I connecting the SPI the above pic is the error
[10:27:29] Status: Failed, Error Type: RADAR INTERFACE ERROR
[10:27:33] MSS Power Up async event was not received!
Request for Assistance:
Could anyone guide me on what steps I should take next to debug this issue? I'm looking for any common troubleshooting tips or specific steps that might help resolve this connectivity problem.
Thank you in advance!
Best regards,
Balu