The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A22362: Does the part has default mode when power off

Part Number: TS5A22362
Other Parts Discussed in Thread: TS5A23159

End user send information to us that they test TS5A22362 COM is connect to NC or NO  when the audio source hasn't power on.

I see the part doesn't suggest com folat and NC ,NO float at design.

does the com connect to one output channel NC or NO as the part default mode or the part has no high resistense mode, the COM and NC, NO couldn't divide at same time.

  • Lanjie,

    The TS5A22362 switch state is not defined with Vcc = 0 V.  If you would like to guarantee defined Hi-Z state when Vcc = 0 V you will need to select a device with powered off protection feature.  You can tell if a switch has this feature by looking for a leakage spec with Vcc = 0V like the TS5A23159. 

    Thank you,

    Adam