The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5947: CCS 11.2 on Windows 11 ARM fails during installation of CDC drivers

Part Number: MSP430FR5947

Installed CCS 11.2 on Windows 11 ARM (on Parallels 18 on Mac M1 Max) is failing to install.

Specifically the installer gets to the stage where it tries to install certificates (and succeeds) and then attempts to install the CDC driver for Windows.

I've manually tried this step by running the following:

c:\ti\ccs1120\ccs\ccs_base\emulation\drivers\msp430\DPInst>DPInst64.exe /c /se /sa /path "C:\ti\ccs1120/ccs/ccs_base\emulation\drivers\msp430\USB_eZ-RF"

Notice that I disabled the `/lm` switch (for legacy) mode but there is no difference - driver installation fails in both cases.  I've attached a ZIP of the logs from this process.

Attached are logs from the installation (used set debug=true for the second install).  Let me know what additional information is needed to troubleshoot this.

4201.install_logs.zip