I'm trying to get CCS installed on a new computer with a previously used Stellaris Launchpad (LM4F). CCSv5 is giving me licensing issues. Shouldn't I have a "free" license entitled to me as long as I have the launchpad plugged into my computer? After attempting to debug a program I get "CCS could not find a valid license. A 30-day evaluation license will be generated." It then redirects me to a browser but I get an error there stating "There is currently a problem with the Part Number being Activated. Error Number 10044. Click here to contact us.".
Any suggestions here? I can't get a definitive answer anywhere on the licensing of CCS with a purchased Launchpad. This is CCSv5 download that is bundled with StellarisWare.