This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO 4.1.3 + TMS320DM6446 Icepick: >>> Error 0x80000260/-1137

Other Parts Discussed in Thread: TMS320DM6446, CCSTUDIO

Hello,

I am getting Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4 following error message when I try to connect

TMS320DM6446  on Code Composer 4.1.3.

It works fine on CCStudio 3.2.

I am using Spectrum Digital 510USB.

=========== Error ====================

Error connecting to the target:
Error 0x80000260/-1137
Fatal Error during: Execution, Initialization, OCS,

It appears that the target is being held in reset.  This may be
due to Wait-In-Reset (WIR) configuration set by the EMU0=0
and EMU1=1 pin settings.  If this is the case, DISCONNECT
all CONNECTED devices including icepick and then select
RETRY to clear the WIR configuration.

If this is a multi-core system, the master CPU may not be
releasing the DSP/MCU from reset.  Please check your
configuration in CC_setup and/or your GEL file to ensure that
nothing is blocking the DSP/MCU from being released from reset.

========================================

Any help is appreciated!

Sid