The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100V2 USB emulator do not connet to TMS320DM6467 at all

I am using JTAG XDS100V2 USB emulator 14 pins for da vinci processor the DM6467T DIGITAL VIDEO EVALUATION MODULE. I am using Code Composer V4 downloaded from TI page and updated. The software runs under Windows XP.

I am connecting properly the JTAG to the board and to the USB port of the computer. I programed a simple code of "hello word" and it is compiling properly but I am getting the following error:

Error connecting to the target:

 

Error 0x80000260/-1137
Fatal Error during: Execution, Initialization, OCS,
It appears that the target is being held in reset.  This may be
due to Wait-In-Reset (WIR) configuration set by the EMU 0/1 pin
settings.  If this is the case, press Cancel and disconnect all
connected devices to attempt to clear the WIR configuration.

EMU 0/1 pins are both set to high


Can anyone help ?
Thank you