Other Parts Discussed in Thread: BOOST-CCEMADAPTER, CC3200, CC256XCQFN-EM, CC3200AUDBOOST
My setup:
CC2564C
MSP432P401R launchpad
BOOST-CCEMADAPTER
CC3200 AudBoost
Code Composer Studio Version: 10.4.0.00006
BT Stack: CC256XMSP432BTBLESW_4.2.1.1
I would like to simulate a Headphone function connected with a phone for Eg. I would like to use functions like:
1)Anser the call / Cut the call (with button)
2) Volume up/ Down (with buttons of course)
3) send some two-way 2- char data in ASCII format.
4) Is there a way to play a short beep sound if the bT device is connected / Disconnected? if so explain in brief
If I understand well. I need to combine 2 or more BT Classic profiles. HFP& SPP; HFP for purpose 1, SPP for purpose 3, and which profile should I use for purpose 2? & 4?
other suggestions of what audio codec be used / MCU suggestions (battery operated applications) etc.
I've tried the default examples stated in the documents of this individually "User’s GuideCC2564x Demo Applications" All the examples works individually with no issues! now, how can I combine the profiles and use them to gather?
My 3rd purpose is to use an existing BT device(cannot change this method) that resumes Audio call streaming to my device if I send some custom char(cannot change this either preset custom ASCII Char) via BT like writing in the console for eg.
How can I achieve this 3rd purpose? & all of my purposes Together 1,2,3,4?
Please explain me in a brief rookie to BT Domain. How can I combine & use two or more BT Classic profiles at once? how to achieve this? please explain & really appreciate your answers and Time.
Any examples will also be appreciated
Thanks a Lot.