This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] BLE Qualification : Known Issues and Fixes [Updated July 2021]

Guru 57865 points
Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2650MODA, CC2650, CC2640, CC1350, CC2640R2F

Please see this thread for Bluetooth Qualification updates.

CC2640R2F / CC26X0 / CC13X0

Additional documentation for CC2650MODA

0572.cc2650moda.zip

Erratum 10734

Customers attempting to create an End-Product listing with our qualified UUIDs, may end up with inconsistencies due to TCRL 2018-1 (Erratum E10734).

For CC2640R2, attached here are test evidence needed to complete the listing; 

And here are the test reports:

For CC2640 / CC2650 / CC1350:

These test evidences are based on Category B  which means that they were collected by in house testing (Not PTS). Sniffer and logs must be shared with the end-product listing. Here is an example how;

For Peripheral:

Test Evidence Information

Test Case Verdict (Pass, Fail,  Waived, Referenced)

Test Execution (Date)

Test Equipment Platform

Test Report Reference

IUT Configuration

Integrated QDID

Evidence Notes

Pass

28/03/2019

CC2640R2F

BLE5-1.1.3

D041506

 

For Peripheral+Central:

Test Evidence Information

Test Case Verdict (Pass, Fail,  Waived, Referenced)

Test Execution (Date)

Test Equipment Platform

Test Report Reference

IUT Configuration

Integrated QDID

Evidence Notes

Pass

28/03/2019

CC2640R2F

BLE5-1.1.3

D041507

And here are the test reports:



Erratum 11838

CC1350:

CC2650:

CC2640R2F (BLE Stack):

CC2640R2F (BLE5 Stack):

CC26x2 / CC13x2

Erratum 10734

For CC26x2/CC13x2, attached here are test evidence needed to complete the BT5.0 listing; 

Erratum 11838

GATT/SR/GAW/BV-11-C

/cfs-file/__key/communityserver-discussions-components-files/538/GATT_2D00_SR_2D00_GAW_2D00_BV_2D00_11_2D00_C.zip

 

HCI/CCO/BV-18-C

Please consult this thread.

     If you are new to the topic and want to learn more on how to qualify your Bluetooth low energy product, please refer to this app note.

     

    This thread has been edited by someone who was not the original author. -Clément