Part Number: CC2640
Other Parts Discussed in Thread: CC2650
Tool/software: Code Composer Studio
Hello,
I use the "simple_peripheral_cc2650_em" as the basis of a project.
Firstly, I launched the stack and then launched the app for the first time and it worked perfectly, and I could connect with nRF scanner. But when I try to launch the app a second time I have some errors :
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Command=20 -- addr=0x00002000 -- length=0x00001000
Cortex_M3_0: File Loader: Memory write failed: Timed out waiting for target flashloader to execute command.
Cortex_M3_0: GEL: File: C:\Users\Public\Workspace_Max30101_2\simple_peripheral_cc2650em_app\FlashROM\simple_peripheral_cc2650em_app.out: Load failed.
So, I checked these two boxes :
Run--> Debug Configurations --> Target: "Reset the target on a connect" and "Reset the target on a program load or restart"
It launches correctly, but then I can't see anything on nRF Scanner. I guess it's because the stack is also reset, so I can't make it works like that.
Do you have any ideas why I can't launch twice without resetting the device ?