My SDK version is : 3_40
IDE Tool: CCS 9.1.0
Using Example: examples\rtos\CC2640R2_LAUNCHXL\ble5apps\simple_serial_socket_server
Question:
Now we using the Flag:-DPTM_MODE to switch the cc2640r2f to run in PTM mode or non-PTM mode.
But now we must burn-in different files to switch PTM mode and non-PTM mode.
Does have any way that I build non-PTM mode, but can via some method to change to PTM mode?
I search in TI Forum, someone is discussing about the HCI_EXT_EnablePTMCmd. Seems if I pull-up a PTM gpio(GPIO_23), then I can send the HCI Command via UART?
Dose anyone knows the relevant information? Please share with me, thanks a lot!