Tool/software:
1. Do I need to write the MAC address of WIFI and BLE separately in CC3351? Can the same MAC address be used?
2. Whether CC3351 support a runtime configurable WI-FI MAC address?
3. Whether CC3351 be able to automatically detect the country in which the appliance is, in order to configure the allowed Wi-Fi country settings using the Linux regulatory database?