Tool/software: Code Composer Studio
Hi,while i modify the email demo to add http get function to download file from the HTTP SERVER and compile the project ,the error will show in the console of
the CSS.
i just add the include header in the main file , such as the below:
a.
// HTTP Client lib
#include <http/client/httpcli.h>
#include <http/client/common.h>
b.and include Options in the Properties->Build-> ARM Compiler->Include Options
c.and the file path in the Properties->Build-> ARM Linker->File Search Path
as i compile the project ,the error will show ,while i click the erro info on the console ,it will come to SDK directory to the file socket.h
the error show below :
i don't know how to correct this essuse. some sugestion will be helpful.
best regards.