Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

Have you ever seen the wheels on a car actually spin backward while the car is moving forward? Barring an extreme stunt, I’ll bet you probably saw it in a car commercial. Have you ever wondered why?

Real life happens in continuous time, but a video camera can only record a limited number of frames per second. Each frame may capture the wheels in a different position, so depending on how many rotations the wheels complete between frames, they might actually appear to be rotating backward as you watch the video! This effect is known as aliasing.

Data-acquisition systems using analog-to-digital converters (ADCs) experience this same phenomenon as they make discrete “snapshots” of a continuous time signal. In this post, I’ll introduce what aliasing looks like in the world of ADCs. 

Classic example of aliasing in car commercials

Figure 1: Classic example of aliasing in car commercials

What is aliasing?

According to the Nyquist theorem, an ADC must sample the input signal at least twice as fast as its highest-frequency component in order to reproduce the original signal in the digital domain – otherwise, aliases are produced. This minimum required sampling rate is known as the Nyquist rate. Or conversely, the highest-frequency signal that an ADC can accurately convert is one-half the sampling rate, known as the Nyquist frequency.

Let’s take a look at an example data-acquisition system with an ADC sampling a 6-Hz input sine wave at 7 samples-per-second (SPS). Our resulting Nyquist frequency is 3.5Hz, with any input signal frequencies greater than 3.5Hz generating aliases of the original input. Figure 2 illustrates what this looks like in the time domain using the original 6-Hz input and two of its aliases: 1Hz and 8Hz. Since all three sine waves intersect at each sample, a 6-Hz sine wave sampled at 7SPS will look no different than a 1-Hz or an 8-Hz sine wave! When we look at the output data, aliasing makes it impossible to differentiate the 6-Hz sine wave we wanted to measure from its aliases and the desired signal content is lost.

Aliasing in the time domain

Figure 2: Aliasing in the time domain

But how could you have known that a 6-Hz sine wave would have aliases at 1Hz and 8Hz? Looking at aliasing in the frequency domain makes this more apparent. When sampled by an ADC, the frequency content of the input signal repeats itself at multiples of the sampling rate, starting at DC. Now you can see why the term “folding back” is often used to describe how signals alias – if you were to fold Figure 3 at the dotted lines, these signals would overlap each other perfectly.

Aliasing in the frequency domain

Figure 3: Aliasing in the frequency domain

To properly measure an input sine wave, the sampling rate must satisfy the Nyquist sampling criteria. In the example above, you would need to increase the sampling rate to at least 12SPS. At exactly 12SPS, the 6-Hz input will still fold back to DC and add an offset to the measurement, so sampling just a little faster ensures that your signals of interest do not alias at all.

But what about noise? White noise occurs across all frequencies, so it will undoubtedly alias from higher frequencies back into the passband between DC and the Nyquist frequency. The result is a higher in-band noise level, which will degrade important specifications like signal-to-noise ratio (SNR). Fortunately, there’s a solution for that: the anti-aliasing filter.

Anti-aliasing filters

Most ADCs are preceded by an anti-aliasing filter, which is nothing more than a low-pass filter used to attenuate signals beyond the bandwidth of interest. The response of an ideal anti-aliasing filter is perfectly flat up until the Nyquist frequency, after which it rolls off sharply to attenuate out-of-band frequencies as shown in Figure 4. Here, the sampling rate has been doubled to 14SPS, which puts the Nyquist frequency at 7Hz and the original 6-Hz input safely within the passband.

Frequency response of an ideal anti-aliasing filter

Figure 4: Frequency response of an ideal anti-aliasing filter

Designing a filter that can achieve this type of frequency response can be very challenging, often requiring active components. These extra components significantly add to the size, cost, and power consumption of the signal chain and make implementing such a filter far less ideal.

To make this easier to understand, I’ll show you in a follow-up blog how delta-sigma ADCs significantly relax the design requirements on your anti-aliasing filter. Additionally, I’ll provide some key guidelines to designing an anti-aliasing filter that’s appropriate for your application.

Additional resources

Anonymous
  • Hi Hari,

    Even for DC inputs, the goal of an antialiasing filter remains the same - limit the bandwidth of the signal chain by attenuating out-of-band signals without interfering with the frequencies of interest. Just because you are measuring DC content, however, doesn't mean you need to set an ultra-low filter cutoff, nor should you for a couple reasons:

    1. Real-world RC filters begin rolling off very early, so it is generally recommended to keep the -3dB point at least a couple decades beyond your frequencies of interest.  Also, the lower your make the filter cutoff, the larger the passive components typically become, which can introduce other types of errors in your measurement (i.e. large resistors introduce offset in the presence of input bias currents).

    2. The digital filter in delta-sigma ADCs can help a lot with attenuating out-of-band noise. The output data rate can often be chosen such that the digital filter -3dB cutoff is very low (< 1Hz in some devices like our ADS1262). The response of these filters begins at 0dB and repeats at multiples of the modulator frequency (fMOD). The primary goal for your antialiasing filters then becomes to attenuate the noise around n*fMOD only; otherwise, noise in that range will fold back into your passband. This means your RC filter cutoff can be set further in frequency and the response can be more gradual.

    I have a couple more blogs on this very topic; check them out if you're interested!

    Regards,

    Ryan

  • Hi Ryan,

    Could you please tell me how anti aliasing filters behave to a DC input. How to select filter cut off frequency for DC inputs.

  • It's easy to see pictorially that sampling a signal at twice its rate will not yield its frequency.  Draw a sine wave and mark samples every 180 degrees.  It doesn't matter where you start, from symmetry, all the points will add to zero.

  • :

    Hi Ken,

    I agree, there are inconsistencies amongst a number of definitions out there as to whether the '=' is included or not. In the end, I hope it's clear that sampling at exactly 2*fmax is generally insufficient and therefore impractical in most ADC applications.

    Thank you both for your comments!

  • I agree with Donald.

    The problem I have seen is that there are inconsistencies between text books. Some will state that the Nyquist Rate is 2*fmax >= fs while others will state 2*fmax > fs. I have always been taught that the sampling rate must be more than twice the maximum frequency of interest. Oppenheim & Wilsky, Signals & Systems states this (see page 519).

    In fact, Tim Wescott from Wescott Design Services posted a paper on this very subject some time ago, "Sampling: What Nyquist Didn't Say And What To Do About It."