Hello,
I'm testing with the TPS61086 in combination with BQ24075 and TPS54318. the TPS61086 I like to use in our apllication for 5V and 12 V the TPS 54318 for 3,3 V.
Everything works fine excapt one thing. when i like to shutdown the output on the TPS61086 ( with the J7) the 12 V is going down to 4 a 5 Voltage but don't go to 0V.
I have connect a big resistor of 20 ohm to the output.
The TPS54318 will do this perfect.