This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler installation and selection in CCE v3



It appears that CCEv3 does not allow users to add/select newer versions of MSP430 codegen tools like we do in CCS v4, as documented in http://tiexpressdsp.com/index.php/Compiler_Installation_and_Selection

In CCE3, under Window->Preferences->C/C++->TI Code Generation Tools, it does allow you to add and "Extended Code Generation Tools Discovery Path", however the new version is not "recognized". I have tried it and can't get it to work. It appears that this functionality is just not enabled in CCE3. Is there a setting or some way to enable this for users to use a newer version of CGT with CCE, or do they pretty much have to move to CCSv4 to avail of this functionality?

 

  • Aarti,

    CCE has the functionality but it probably doesn't recognize a more recent version of CGT.  For a particular version class (3.0.x or 3.1.x) CCS needs a build options plug-in.  It likely doesn't have the plug-in for the version you are trying to discover.

    John

     

  • Thanks John. That must be it. I was trying to get it to recognize 3.2.x versions and it couldn't. I'll ask the customer to move to CCS4 if he needs to use these newer CGT versions.