you cannot run WOR if you have powered down the RC oscillator. This is controlling the sleep timer that makes sure that the radio wakes up from Sleep.
Without the RC oscillator running, the radio should draw about 0.2 uA is you put it into SLEEP (SPWD…
Part Number: CC1101 Other Parts Discussed in Thread: TEST2 Dear Team, I am currently utilizing the CC1101 chip, where I have initiated the power-down mode by implementing the following configuration:
void CC1101_PowerDown()
{
SpiStrobe(CC1101_SIDLE…
Hi Felipe,
This is a very interesting conversation and I would be interested to know how well this works for you.
We have been using the CC1200 to receive bi-phase encoded data starting with FFFE for many years, but have used the CC1200 just as an 'RF…
I do not understand what you are doing in the code you have provided, and I am unsure what you are asking about in the post.
In the code you are for example writing to 59 registers, but I gave you a list of 26 register you should use?
Why are you writing…
Part Number: CC1101 Other Parts Discussed in Thread: CC1150 Hi experts,
Some of the products my customers mass produce communicate in the 315MHz frequency band using CC1150 as a transmitter and CC1101 as a receiver. Could you please answer the following…
Hi,
With the CC1101, the best option would be to use the 868 MHz balun; which goes into a SPDT switch. With the "A" switch option, there should be a 433 MHz LPF and on the "B" switch option there should be a 868 MHz LPF. Then these signals should…
Part Number: CC1101 Hi, In the SWRA468, it is mentioned to use a Ref Unit Receiver. My question is: can we consider any TI EM as a reference and deem it as the golden standard, or should we purchase the one that has been tested by TI?
Thnaks, Babak
Part Number: CC1101 If the CARRIER_SENSE_ABS_THR is disabled (0x08) would the MAGN_TARGET settings have any effect for the RF performance, or would it also be essentially disabled?